2024-01-02 3:05 AM - edited 2024-01-02 3:08 AM
Hi, i am using Timers to control the intensity of a RGB LED. I need help with a code because I don't know why i have to do this thing.
I have these lines:
TIM1->CCR1 = Intensity; For Red Color
TIM1->CCR2 = Intensity; For green color
TIM1->CCR4 = Intensity; For blue color
but it doesn't work while calling
(&htim1, TIM_CHANNEL_4);
But if i do this:
// Set alternate output for CH2, disabling main output (no need of it because already disabled, but just in case)
CLEAR_BIT(TIM1->CCER, 1 << 4);
SET_BIT(TIM1->CCER, 1 << 6);
// Set alternate output for CH1, disabling main output (no need of last thing but whatever)
CLEAR_BIT(TIM1->CCER, 1 << 0);
SET_BIT(TIM1->CCER, 1 << 2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_4);
It starts working. This last code is not mine, this is why i am asking this. Why i have to use clear bit, and do this shifts? I have no idea with this.
Thank you so much.
Solved! Go to Solution.
2024-01-02 6:09 AM
Hello,
Based on GPIO configuration, it seems you are using CH1N, CH2N and CH4 channels of TIM1. Therefore, CH1 and CH2 didn't need to be enabled. However, CCER, 1 << 4, CCER, 1 << 6 are used to disable CH2 channel and enable CH2N which normally not required.
You should have the following startup sequence:
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_4);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);Is working well on my side.
Best Regards,
Gwénolé
2024-01-02 5:31 AM
Hello @rubenles,
TIM1->CCR1 = Intensity; For Red Color
TIM1->CCR2 = Intensity; For green color
TIM1->CCR4 = Intensity; For blue color
I guess those lines are used during TIMER configuration. It allows to select the pulse width for each channel.
Could you share your configuration function? Could you also that channels 1 & 2 are already setup before starting channel 4?
Best Regards,
Gwénolé
2024-01-02 5:46 AM
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(timHandle->Instance==TIM1)
{
/* USER CODE BEGIN TIM1_MspPostInit 0 */
/* USER CODE END TIM1_MspPostInit 0 */
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**TIM1 GPIO Configuration
PE8 ------> TIM1_CH1N
PE10 ------> TIM1_CH2N
PA11 ------> TIM1_CH4
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF1_TIM1;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF1_TIM1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);My doubt is why to do CCER, 1 << 4, CCER, 1 << 6, and those lines.., the configuration i think it's ok.
2024-01-02 6:09 AM
Hello,
Based on GPIO configuration, it seems you are using CH1N, CH2N and CH4 channels of TIM1. Therefore, CH1 and CH2 didn't need to be enabled. However, CCER, 1 << 4, CCER, 1 << 6 are used to disable CH2 channel and enable CH2N which normally not required.
You should have the following startup sequence:
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_4);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);Is working well on my side.
Best Regards,
Gwénolé
2024-01-02 10:23 PM
I tried to do what you said deleting my shift lines and it works but not perfectly...
When i use TIM1->CCR2 = 500; it switches on the green color that is right, when i use TIM1->CCR4 = 500; blue color switches on, but, when i use TIM1->CCR1 = 500; it has to switch on to red color but the result is an strange green.
Using the code i sent before, using CCR1 shows red color, and now it hasn't. What it could be?
Thank you so much, i think i am near the final solution!!
2024-01-03 1:11 AM
@GwenoleB Fixed, i have other line of CCR2 in other place of the code, i was crazy looking for the error. The thing you tell me works perfectly!! Thank you so much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.