2020-06-22 7:47 AM
In a particular time critical application, I'd like to use the LL driver only, FreeRtos and, to preserve an hw resouce, I've selected "none" in SystemCore->Sys->TimeBaseSource.
Trying to compile the project generated in this way, I get "fatal error: stm32g0xx_hal.h: No such file or directory", even if I don't use hal at all.
If I delete the file stm32g0xx_hal_gpio.c from source, the project compile correctly, but if I rebuild the project from the ioc, the file is created again and the error is the same.
Step to reproduce the problem:
STM32CubeG0 Firmware Package V1.3.0
STM32CubeIDE Version: 1.3.1 Build: 6291_20200406_0752 (UTC)
Thank You in advance
Paolo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.