2023-09-20 6:26 PM
Using the latest STM32CubeIDE 1.13.2, it's giving errors compiling a STM32469I-DISCO 32F469IDISCOVERY project, i.e. GPIO_EXT example. This project was imported by STM32CubeIDE from STM32Cube_FW_F4_V1.27.1\Projects\STM32469I-Discovery\Examples\GPIO\GPIO_EXTI\SW4STM32.
The 4 errors are like below. Is this a problem with the project or with STM32CubeIDE? Thanks
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626\tools\arm-none-eabi\bin\ld.exe: C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-closer.o): in function `_close_r':
(.text._close_r+0xc): warning: _close is not implemented and will always fail
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626\tools\arm-none-eabi\bin\ld.exe: C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-lseekr.o): in function `_lseek_r':
(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626\tools\arm-none-eabi\bin\ld.exe: C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-readr.o): in function `_read_r':
(.text._read_r+0x10): warning: _read is not implemented and will always fail
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeIDE_1.13.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626\tools\arm-none-eabi\bin\ld.exe: C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-writer.o): in function `_write_r':
(.text._write_r+0x10): warning: _write is not implemented and will always fail
Finished building target: STM32469I_DISCOVERY.elf
18:56:16 Build Failed. 4 errors, 4 warnings. (took 4s.765ms)
2023-09-20 7:56 PM
There was an upgrade to the toolchain with the recent version which is causing these warnings. See here for some good answers on why exactly this is happening:
At its core, this is probably something that will get resolved in the next STM32CubeIDE version.
> Finished building target: STM32469I_DISCOVERY.elf
As you can see, these are warning, not errors, and the code compiles. You can ignore them if you want.
2023-09-21 5:50 AM
Hello @testcode99 ,
I confirm the issue and I reported internally.
Internal ticket number: 161907 (This is an internal tracking number and is not accessible or usable by customers).
Sorry for any inconvenience and thank you for your contribution in STCommunity :).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.