2022-11-09 4:20 AM
I am trying to create a first Unit Test with Ceedling/Unity/CMoke for my STM32CubeIDE project.
The project has started building but getting an error:
-----------
Linking test_functions_STM32G474RB.out... /Applications/STMicroelectronics/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.macos64_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld: warning: cannot find entry symbol Reset_Handler; defaulting to 0000000008000000 Running test_functions_STM32G474RB.out...
ERROR: Test executable "test_functions_STM32G474RB.out" failed.
Produced no final test result counts in $stdout: sh: build/test/out/test_functions_STM32G474RB.out: No such file or directory And exited with status: [0] (count of failed tests). This is often a symptom of a bad memory access in source or test code.
rake aborted!
----------------
This is the project.yml file:
---
# Notes:
# Sample project C code is not presently written to produce a release artifact.
# As such, release build options are disabled.
# This sample, therefore, only demonstrates running a collection of unit tests.
:project:
:use_exceptions: FALSE
:use_test_preprocessor: TRUE
:use_auxiliary_dependencies: TRUE
:build_root: build
# :release_build: TRUE
:test_file_prefix: test_
:which_ceedling: gem
:ceedling_version: 0.31.1
:default_tasks:
- test:all
#:test_build:
# :use_assembly: TRUE
#:release_build:
# :output: MyApp.out
# :use_assembly: FALSE
:environment:
:extension:
:executable: .out
:paths:
:test:
- +:test/**
- -:test/support
:source:
- Core/Inc/**
- Core/Src/**
- Core/**
- Drivers/CMSIS/Device/ST/STM32G4xx/Include/**
- Drivers/CMSIS/Include/**
- Drivers/STM32G4xx_HAL_Driver/Inc/**
- Drivers/STM32G4xx_HAL_Driver/Inc/Legacy/**
:support:
- test/support
:libraries: []
:defines:
# in order to add common defines:
# 1) remove the trailing [] from the :common: section
# 2) add entries to the :common: section (e.g. :test: has TEST defined)
:common: &common_defines []
:test:
- *common_defines
- TEST
:test_preprocess:
- *common_defines
- TEST
:cmock:
:mock_prefix: mock_
:when_no_prototypes: :warn
:enforce_strict_ordering: TRUE
:plugins:
- :ignore
- :callback
:treat_as:
uint8: HEX8
uint16: HEX16
uint32: UINT32
int8: INT8
bool: UINT8
:includes:
- <stdbool.h>
- <stdint.h>
:treat_externs: :include
# Add -gcov to the plugins list to make sure of the gcov plugin
# You will need to have gcov and gcovr both installed to make it work.
# For more information on these options, see docs in plugins/gcov
:gcov:
:reports:
- HtmlDetailed
:gcovr:
:html_medium_threshold: 75
:html_high_threshold: 90
#:tools:
# Ceedling defaults to using gcc for compiling, linking, etc.
# As [:tools] is blank, gcc will be used (so long as it's in your system path)
# See documentation to configure a given toolchain for use
:tools:
:test_compiler:
:executable: arm-none-eabi-gcc
:arguments:
- '${1}'
- '-mcpu=cortex-m4'
- '-std=gnu11'
- '-g3'
- '-DDEBUG'
- '-DUSE_HAL_DRIVER'
- '-DSTM32G474xx'
- '-c'
- '-I Core/Inc'
- '-I Core/Startup'
- '-I Drivers/STM32G4xx_HAL_Driver/Inc'
- '-I Drivers/STM32G4xx_HAL_Driver/Inc/Legacy'
- '-I Drivers/CMSIS/Device/ST/STM32G4xx/Include'
- '-I Drivers/CMSIS/Include'
- '-I #{Ceedling.load_path}/../vendor/unity/src'
- '-I Core/Startup'
- '-O0'
- '-ffunction-sections'
- '-fdata-sections'
- '-Wall'
- '-fstack-usage'
- '--specs=nano.specs'
- '-mfpu=fpv4-sp-d16'
- '-mfloat-abi=hard'
- '-mthumb'
:test_linker:
:executable: arm-none-eabi-gcc
:arguments:
- '-o "STM32G474RB - PLATFORM.elf"'
- '-mcpu=cortex-m4'
- '-T"/Users/raul/Documents/repository/platform-firmware-c/STM32G474RB - PLATFORM/STM32G474RBTX_FLASH.ld"'
- '--specs=nosys.specs'
- '-Wl,-Map="${BuildArtifactFileBaseName}.map"'
- '-Wl,--gc-sections'
- '-static'
- '--specs=nano.specs'
- '-mfpu=fpv4-sp-d16'
- '-mfloat-abi=hard'
- '-mthumb'
- '-Wl,--start-group'
- '-lc'
- '-lm'
- '-Wl,--end-group'
# LIBRARIES
# These libraries are automatically injected into the build process. Those specified as
# common will be used in all types of builds. Otherwise, libraries can be injected in just
# tests or releases. These options are MERGED with the options in supplemental yaml files.
:libraries:
:placement: :end
:flag: "-l${1}"
:path_flag: "-L ${1}"
:system: [] # for example, you might list 'm' to grab the math library
:test: []
:release: []
:plugins:
:load_paths:
- "#{Ceedling.load_path}"
:enabled:
- stdout_pretty_tests_report
- module_generator
...
--------------------------
I have tried to add the .S file on the compiler/linker flags. But, either I am doing it wrongly or it doesn't work.
I would really appreciate that somebody with more experience than me could point what I am doing wrong.
Thanks in advance.
2022-11-10 1:35 PM
For future visitors, if can be of any help…
I ended up using the gcc compiler instead of the arm one. I removed the HAL drivers and the rest of the source files from the :source: includes. Then I created a separate .h and .c with the code I wanted to test. Then I had to mock up a few included headers with the minimum required functions and variables to be able to build the test code. The functions and the variables were in some cases adjusted/mocked to make it work.
Good luck…
2023-01-27 12:58 AM
It looks like the linker is missing the startupcode, where reset_handler is a part of and which is provided via the startup...s file.
the .s file must be compiled with arm-none-eabi-as and not with arm-none-eabi-gcc, so maybe you are missing this in your ceedling project settings.
But you can also provide the startup Code in C. For STM32H7 (that is the SoC i work on) i found this repo: https://github.com/elzoughby/STM32H7xx-Startup/blob/master/src/startup_stm32h743xx.c
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.