2024-12-20 7:22 AM
I am trying to build the toolchain and I'm looking for some help getting over this hurdle.
When I run build-prerequisites.sh on Ubuntu, it stops when it tries to run "helper.py" with the error "You need to install python-magic." Helper.py is running python3 which I've tried linking to Python3.4, 3.5, 3.8, etc. If I change it to use Python2, it gets over this error but fails with a different one regarding a FILE==STDERR parameter being passed to the Print function (I'm not a Python guy).
Just starting Python2 and typing the line "Import Magic" works. Any other Python does not work.
Let me also put out that what I am really trying to do is get the sources for all the running code so when I debug I can debug into the function. It might be that I can just take that "src" directory and park it somewhere and get the same result, but it's more figuring out than I have time for.
I only need the build for Windows also and I assume I need the "debug" type but there is zero documentation.
The version I downloaded from GitHub is this:
Release GNU Tools for STM32 12.3.rel1.20240926-1715
Thanks in advance for your help.
donkharrison
2024-12-20 8:34 AM - edited 2024-12-20 8:40 AM
> it stops when it tries to run "helper.py" with the error "You need to install python-magic."
It is available here: https://pypi.org/project/python-magic/
> what I am really trying to do is get the sources for all the running code so when I debug I can debug into the function.
So you need to build only the newlib. Even do not build it, maybe just looking at the sources can be enough.
2024-12-20 9:40 AM
I have installed python-magic, but when I am running python3, it will not execute "Import magic."
I'm not sure what newlib is other than what Wikipedia told me, or how I would use it. I can see that it is part of the build, and I can see that I can make it independent of the build (seemingly).
In the end, I need the STM32CubeIDE to have access to the sources when I single step outside the scope of my code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.