STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Questions about coding style

Hello,I want to get the coding style of the SDK so that my code is consistent with the style of the SDK.Can you provide the appropriate configuration file?

Bug: STM32CubeIDE deletes files on Code Generation

STM32CubeIDE v1.0.1 deletes all my project files when I'm generating code with the integrated CubeMx. This only happens when theres a wrong path set in settings under firmware update.It then shows me the following error. When I then click on OK, I se...

0690X000009YiKYQA0.png
thejc by Associate II
  • 2421 Views
  • 3 replies
  • 0 kudos

How to compile example packet X-Cube-SPN8?

Hi, I am trying to manage a BLDC motor using the P-Nucleo-IHM001, so NucleoF302R8 and X-Nucleo-IHM01M1.I would like to upload the firmware version with the example X-Cube-SPN8.When I launch the building, it gives errors due to a different path, that ...

Update ARM toolchain in STM32Cube IDE

Hi,I wonder if it is possible to add/update manually the toolchain ARM?Currently it is only 7-2018-q2 while there is the 8-2018-q4 available.I wanted to use the latest one.Any ideas?Thanks in advance,Kind regards,Anthony

ABern by Associate II
  • 2329 Views
  • 2 replies
  • 0 kudos

SWV not working with STM32CubeIDE

Serial wire viewer is not showing since STM32CubeIDE version 1.0.1. It has worked before in version 1.0.0.I'm trying to use it with a STM32F103RBT6 but also tried it with a Nucleo F103RB.The live Expressions work perfectly fine, but not the SWV it ju...

0690X000009YQRbQAO.jpg 0690X000009YQRMQA4.jpg
thejc by Associate II
  • 3326 Views
  • 3 replies
  • 0 kudos

headless build fails when saving workspace

Hi all,I hope someone will be able to help me out. I want to compile my STM32CubeIDE project. It works but when it is saving the workspace, it returned an error. See below: Saving workspace.Stm32cubeidec:Java was started but returned exit code=1any i...

ABern by Associate II
  • 2467 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.