STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to install an Eclipse CDT Plugin like OpenMRC?

Dear Friends, I'm having problems to load this plugin (Eclipse CDT Plugin: OpenMRC), it's from GitHub, I tried using the "Install New Software" but without good results, I also download it to my desktop but the IDE wants JAR files, so please someone ...

0690X00000A9k26QAB.jpg
HLare by Associate
  • 2297 Views
  • 2 replies
  • 0 kudos

Where is the C++ support in STM32CubeIDE?

When starting a new project in STM Cube IDE there is an option given to generate C++ instead of C code but when selected I still get the same generated c code... If I wan't to use modern C++ conventions what are my options or should I be looking at a...

norlesh by Associate III
  • 2223 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeIDE library inclusion error !!!

I downloaded the X-NUCLEO-IHM01A1 from the st website and loaded an example project in stm32cubeIDE, however I keep on getting the library inclusion error.

0690X000009YpmRQAS.png
Cash by Associate II
  • 1538 Views
  • 1 replies
  • 0 kudos

Device Configuration Tool Resets Project Properties.

Hi,I upgraded to the latest version of STM32CubeIDE (Version: 1.0.2) and I am noticing a possible bug with the device configuration tool. Whenever I open the tool and generate code from it, it resets all my build and general properties. This is reall...

PShut by Associate
  • 952 Views
  • 0 replies
  • 1 kudos

LD1 (LED1) is not defined for device NUCLEO-H743ZI board STMCubeIDE version 1.0.2 STM32CubeH7 MCU Package 1.5.0

LD1 is not defined in device NUCLEO-H743ZILD2 and LD3 both seems ok.also, the builtin flash tool doesn't have the latest firmware for the stlink v2had to flash with the tool found here to get debug working:https://www.st.com/en/development-tools/stsw...

How to update/reflash firmware rather than Debug ?

Hi all,I am using STM32Cube IDE (Eclipse based) and I am trying configure the IDE to reflash the uC using the Run option rather than Debug option, without success.I always used OpenOCD from shell under Linux for this purpose.How can I setup the STLin...

simo zz by Senior II
  • 2053 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.