STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Eclipse Color Themes extension

Hi! So, TrueSTUDIO supports the Eclipse Color Theme extension right out of the box.STM32CubeIDE instead does not, but not only: even after searching for it in the Marketplace, it does not show up. Why?I know that maybe this is not an high priority is...

Lori B. by Associate III
  • 1974 Views
  • 1 replies
  • 1 kudos

Multiple MCU support in a static library project

Some time ago I created a static library project in AC6 System Workbench for STM32. The project expanded and I started to adding build targets for more microcontrollers, STM32L, STM32F7, etc. After migrating the project to Cube IDE I am no longer abl...

0690X000009k2OhQAI.png
MMatu by Associate III
  • 987 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE on MAC Mojave and .dylib ... Resolved!

When I started a debug-session, I got the following message:dyld: Library not loaded: /opt/local/lib/libusb-1.0.0.dylib Referenced from: /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server....

Resolved! With the ADC using single ended input channel, what is the internal vref, what is the 12 bit voltage range for measurement (is it 0 to 2.5V or 0 to 3.3V)? What is the lowest accurate measurement resolution when we have less than 20mV to measure?

I am trying to work with photo diodes and need to measure 20mV or less with ADC. Whats the best resolution I can get with a single ended ADC (using ADC 3 channel 12 at the moment).Whats the measurement range on that channel? When we have less than 10...

PRedd.111 by Associate III
  • 1650 Views
  • 2 replies
  • 0 kudos

How to perform Firmware Upgrade on STM32F413 Discovery Board.

Hi, We are looking to perform a firmware upgrade on STM32F413 where the firmware upgrade image is coming over BLE chip which is interfaced over UART to this controller. Can I know if any procedure was available to perform this operationRegardsSrikan...

Smedi by Associate II
  • 1003 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.