STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

SPI function in STM32091C-Eval using STM32CubeIDE

Hi, I want to use SPI function from the evaluation board to connect to an FPGA. However I see that the MOSI port at pin PE15 at connector CN7 does not response. In Userguide UM1817, Table 23 said, to disconnect with function block on STM32091C-EVAL b...

CubeIDE v 1.1 - problem with SWO debug output

It looks like the CubeIDE debugger (GDB server) has issues with SWO output.When I enable SWO output in debug config and actually print something, only first few lines appear in the SWV ITM data window. Then one of following occurs:Debugger loses conn...

Pavel A. by Super User
  • 1117 Views
  • 0 replies
  • 2 kudos

Problem with nearly new Nucleo F722ZE

New Nucleo-F722ZE initially worked fine (initially prompted for software update). But after approx 3 hours when trying to Run->Debug , it now shows:Waiting for debugger connection...Debugger connectedDebugger connection lost.Shutting down...Power cyc...

STM32F429 Discovery CUBE IDE SWV printf not working

I'm using STM32F429 Discovery board and CUBE IDE. I have set the Serial Wire Debug, in debug configuration, I enabled SWV, set the core clock, enabled live expession. In main.c I wrote this part of the code int _write(int file, char *ptr, int len){  ...

Resolved! Error with auto generated drivers in CubeIDE

I am not sure this belongs here, it could just as well be in MCU, but i believe it could be a configuration problem, so i put it here.I am working on a project with Cube IDE. when I tried to compile for the first time, the build failed because of er...

Ubus99 by Associate III
  • 2240 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.