STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Should CubeIDE 1.3.1 projects open in 1.3.0?

Can someone tell me with absolute certainty whether a workspace and project created with CubeIDE 1.3.1 should (is supposed to) open (and build etc) properly with CubeIDE 1.3.0?I guess it should if only the last digit changed (if that's typical semant...

SKled.1 by Senior II
  • 1331 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE Build Error

Hello my STM32Cube IDE is showing me the build error " program -E not found in the Path". But in the Preprocessor Include Paths, Macros.. window, there is no Provider tab. I have tried to uninstall and installed again but the result is the same.So co...

0693W000001qeyxQAA.png 0693W000001qezWQAQ.png
ATun by Associate
  • 2017 Views
  • 2 replies
  • 0 kudos

How to change VECT_TAB_OFFSET in IDE (MX)

Now, I develop DFU.0x80000000 : DFU Project0x8000C000 : Application Project.I have to change VECTOR Table in Application Area.I'm trying to find VECT_TAB_OFFSET in IDE.But, I can'tOld solution is directly change source code in System_stmf2xx.cI don't...

NH by Associate II
  • 4769 Views
  • 6 replies
  • 0 kudos

CUBEIDE shuts down

My windows 10 CUBE IDE, version 1.3.1 shuts down several times a day. Genarally at the "debug" perspective (the most used). I have been trying to switch "compatibility option" from w-10 down the oldest (windows 7...) and less unsuccessfully.Should I ...

JSILV.2 by Senior
  • 2529 Views
  • 4 replies
  • 0 kudos

Resolved! Problem with NUCLEO-H743ZI2 and STM32CubeIDE debugging

Hello,I have recently bought the NUCLEO-H743ZI2 board and I can't use the on board STLINKV3 debugger with STM32CubeIDE, in ST-LINK GDB Server mode. However I can debug in OpenOCD mode.The error I get is the following:STMicroelectronics ST-LINK GDB se...

IGrag by Associate
  • 3074 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.