STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't install STM32CubeIDE 1.40

I had some trouble to install STM32Cube 1.4.0 and I did a deinstallation via Windows Apps-Tool.Also I delete some Registrieentries.Now I can't Install STM32Cube 1.4.0 viast-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exeWhen I start the exe I getI g...

GAM by Associate II
  • 1229 Views
  • 1 replies
  • 0 kudos

Resolved! What is the official way to open an example project from STM32Cube_FW packages with STM32cubeIDE?

I’ve been using these examples for a long time, but I’ve never been able to open them and rebuild them right after importing without an error or missing path of header and source files. For simple examples, this is not so much a problem, but for more...

STM32Cube apps don't start

Hello,Recently I did a fresh, clean install of macOS Catalina 10.15.6 and I cannot start any of STM32Cube apps.I downloaded STM32CubeMX 6.0.0, STM32CubeProgrammer 2.5.0 and STM32CubeIDE 1.4 and installed them using this commands:sudo java -jar SetupS...

0693W000003BjV8QAK.png
BSewe.1 by Associate II
  • 2718 Views
  • 5 replies
  • 0 kudos

How to uninstall STM32CubeIDE

Hello.I use Debian Buster an I downloaded STM32Cube IDE from here:https://www.st.com/en/development-tools/stm32cubeide.htmlI used the Linux debian package (.deb file) and ran the sh script that comes inside the zip file (version 1.3.0).Since this is ...

May had a bug in STM32CubeIDE V1.4.0

I recently upgraded STM32CubeIDE to version 1.4.0 and opened a previous project in it. After opening the .ioc-File from the project, I noticed that the NVIC-settings had all changed.The settings were correct when I opened this .ioc file with CubeMx v...

Slh by Senior
  • 598 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.