STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! UART1 Configuration for Data Bits(Word Length) 7.

Hi @All ALL​ @Martin KJELDSEN​ I am using STM32F412CGU6 microcontroller.I would like to Configure UART1 with following settings.  • Baud Rate: 9600  • Start bits: 1  • Parity: Even  • Data Bits: 7  • Flow Control: Off  • Stop Bits: 1In STM32CubeMX, T...

Can I use the vl53l1x sensor API without the expansion shield?

I am new to the STM32 and trying to use the vl53l1x sensor. I found a nice article about importing the sensor as below.https://www.digikey.com/eewiki/display/microcontroller/Adding+the+VL53L1X+Driver+to+an+STM32Cube+ProjectHowever, not only above but...

SAn.2 by Associate
  • 1842 Views
  • 2 replies
  • 0 kudos

Unable to connect with my board

I bought new STM32F303VCT6 Discovery board .I connect it to the laptop with using USB user port of the board just for checking it is working or not , after that I saw window pop-up with readme and something and I ignored that referring to user manual...

NPAND.11 by Associate
  • 1249 Views
  • 2 replies
  • 0 kudos

Custom download location to avoid using SSD drive

I am using STM32CubeIDE. It frequently downloads large files from internet (e.g.; device specific file when you start a new project, updates, etc).The problem is, the files are downloaded to my C drive which is SSD. The download location is "C:\Users...

EKarg.1 by Associate
  • 912 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.