STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Memory alignment(structure Padding)

Hi,I am using STM32CubeIDE 1.6.0.In my program for EEPROM read/write I have use structure but its takes too much size because of padding.I tried with #pragma Pack, __attribute__((packed)), even by rearranging the structure member.but there is no size...

Bs.1 by Associate II
  • 2226 Views
  • 1 replies
  • 0 kudos

Resolved! How to change the compiler version on CubeIde

If I want CubeIde to use a specific gnu arm version which is on my local system, should I just setup the build variable "gnu_arm_embedded_compiler_path" ? Is that enough?If I wish to check the current version that cube ide is using, how do I do that?...

DMukh.1 by Associate
  • 10258 Views
  • 2 replies
  • 0 kudos

Resolved! I'm a new user of STM32 (but not new to embedded system design!). I've just upgraded from STM32CubeIDE V1.6.0 to V1.6.1, using a BlackPill STM32F411 target.

The 'reset debug' icon was displayed in V1.6.0 but is no longer visible in V1.6.1. Is this a bug in V1.6.1 or a configuration error of mine? The code is running in the Flash, not RAM (as far as I am aware).Thanks! Mike.

MStev.3 by Associate II
  • 2967 Views
  • 4 replies
  • 0 kudos

Can't run program through CubeIDE.

Normally, I click "Run" in CubeIDE, my program loads onto the Nucleo board and starts running as soon as its loaded. However, in the course of using the debugger, I've somehow messed this up. Now, when I press run, the program downloads correctly, bu...

ASmit.4 by Associate II
  • 1145 Views
  • 0 replies
  • 0 kudos

Resolved! How to write stm32l5xx_hal_mmc DMA to stm32l5xx_hal_ospi?

I’m attempting to optimize a process of loading a large file from eMMC flash memory directly into a SPI device with 8 data lanes. Originally, I meant to use peripheral to peripheral in the DMA component that comes internally with the STM32L5 series. ...

DBark.2 by Associate III
  • 3042 Views
  • 4 replies
  • 0 kudos

Cannot upgrade STM32CubeID or download latest MCU firmware

Cannot upgrade STM32CubeID from 1.5.1 to latest. Always network errors regardless of upgrading inside CubeIDE or trying to manually download the full install from the website.CubeIDE has also migrated by G0 v1.3.0 projects to v1.4.1 and I cannot dow...

SKirk.1 by Associate
  • 1429 Views
  • 2 replies
  • 0 kudos

Window layout

Hello!I'm using the latest 1.6.1 version on Linux Ubuntu.The window layout looks like most of the IDEs I know, source tree on the left (called project explorer), and each source can be displayed in editor on the right and can be rearranged in more wi...

PG.1 by Associate III
  • 1601 Views
  • 1 replies
  • 0 kudos

Instabilities are occurring in Version 1.6.1

I'm using version 1.6.1 in linux, and there are several problems, for example, the main.c file opens but I can't use Delete or BackSpace keys, other times I can't edit the properties of the Device Configuration Tool. It has also occurred that the Dev...

by Not applicable
  • 1053 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.6.1 Update Fails on WIndows 7

I have gotten update notices for STM32CubeIDE 1.6.1 for a couple weeks now. But every time I try to update it fails. I did try deleting the cache directory "STM32CubeIDE\STM32CubeIDE\p2\org.eclipse.equinox.p2.repository\cache" but that did not work...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.