STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Cube ide and qspi

hello we want to use cube debuger in debug whith the qspi. We have some data in the qspi programed by my bootloader or whith the cube programer  Qspi is MX25L51245G we have test them and it is running well the linker QSPI (rx) : ORIGIN = 0x90000000, ...

dacha.1 by Associate II
  • 579 Views
  • 1 replies
  • 1 kudos

MMT area editor bug?

I have problems with using Memory Management Tool (MMT) in CubeMX v6.15.0 and CubeIDE is v1.19.0. MCU is STM32H7R3L8H6H.Here's the MMT view and DTCM area of Boot in focus:As you can see, DTCM area is 64 KB. But in CORTEX_M7_BOOT MPU peripheral view i...

mkrk_0-1758784716889.png mkrk_1-1758784737936.png mkrk_2-1758784818991.png
mkrk by Associate III
  • 843 Views
  • 2 replies
  • 1 kudos

Resolved! CubeIDE malware(orbitum.exe)

When I install and run CubeIDE 1.1.19, it is blocked by KITE Keeper security and cannot be executed. When I asked the server administrator, they said that orbitum.exe runs and prevents it from launching. Is orbitum.exe included in the IDE package?

nalaze by Associate
  • 586 Views
  • 1 replies
  • 1 kudos

Resolved! Cube IDE not showing the login name after successful login

Hi,I have latest version of STM32CubeIDE software . After I logged into the tool, it does not show the user name as it was in previous versions. When I try to login using help -> STM32Cube update -> connect to myST, it says, it will  display message ...

Techn by Senior III
  • 503 Views
  • 2 replies
  • 0 kudos

Resolved! Project Explorer View Disappears

Hi,I have used CubeIDE for 2 years, recently the Project Explorer view disappears occasionally, and I found ctrl-m can recover it, but now it's gone completely, ctrl-m doesn't work, Window->Show View->Project Explorer doesn't work neither.Anybody kno...

Chao by Senior II
  • 986 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Linux IDE display is SMALL on 4k screen

Just download the latest version from ST web and installed Linux version of the STM32IDE tools chain. It is Debian Linux 12, updated and upgraded. No hardware display card. Use the Intel i5 COP internal display card. Display is small on 4k screen. If...

David_ by Senior
  • 1138 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeIDE upgrade

Hello, I have recently upgradated STM32CubeIDE from v.1.13.2 to v.1.14.0.The upgrade seems has gone well, as indicated in the Help->About window:Anyway, if i check the window installed application list, is still indicated the previous version:Also, i...

CTabo1_1-1705396108646.png CTabo1_0-1705396031665.png CTabo1_0-1705396433143.png
CTabo.1 by Senior
  • 5197 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.