STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

empty Map<uint64_t, shared_ptr<CLASS>>. begin() returns NULL

HelloI'm lost.. my code gets HARD-HANDLE due to illegal access, have traced it down to my MAP.but have NO clue to why :(My code have a map of shared pointers. with a key uint64_t.A loop of the elements before any is added makes it crash.now i can see...

M.Holch by Associate II
  • 3407 Views
  • 4 replies
  • 1 kudos

How to include Arduino.h in STM32CubeIDE?

I know this is generally not a kosher move, but I would like to use STM32CubeIDE as well as the Arduino library on one MCU. I need to configure the MCU on a Blue Pill (STM32F103C8) to be an SPI slave. I could not figure out how to get this done in VS...

EPham.1 by Associate
  • 1499 Views
  • 0 replies
  • 0 kudos

BLE project missing files STM32CubeIDE V: 1.7.0

Hello,I'm trying to go through some BLE examples and found some out dated videos on the web. I understand there have been changes over the last year or so but one thing I cannot understand, is missing files.When creating a BLE project in CubeIDE, it...

kcire L. by Associate III
  • 1950 Views
  • 3 replies
  • 0 kudos

Resolved! How to program an SREC during debug?

Our project requires some post-processing of the SREC at compile time. I would like to load the regular ELF file for symbols, but write the SREC to memory. It seems the IDE only accepts ELF files, which I cannot generate. How do I program an SREC ...

BStic.2 by Senior
  • 3736 Views
  • 5 replies
  • 0 kudos

Reset when adding or removing breakpoints

I have a STM32L072 and when last I worked on the project, from what I rmember, there were no debugging issues at all.When I started to work at it again now, I see this effect that, when, in STM32CubeIDE, using a STLINK V3SET debugger, I am in a debug...

SKled.1 by Senior II
  • 4861 Views
  • 8 replies
  • 0 kudos

How to search Project include files.

I am new tp STM32CubeIde and have installed V1.7.0I have loaded a project from the STM32Cube_FW_WL_V1.1.0 example applications.The project explorer shows the project tree with BinariesIncludesApplicationDebug etc nodesIf I use Search->File to open F...

using SPI protocol multi-slave modules with master stm32f1

Hello there,I am working on a project. In the project I want to implement, an external ADC module will collect the data and transfer it to the STM32F103C8. My STM32F103C8 microprocessor will transfer these data to my wireless module. Here I am having...

Hg.1 by Associate
  • 1518 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.