STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Renaming a SMT32CubeIDE project.

I have a project folder named 'myProject' on my hard drive. I want to rename it to 'myProjectOld'. How do I do this in SMT32CubeIDE? I tried using the 'rename' function however it only renames the project in SMT32CubeIDE and not the directory on ...

LMorr.3 by Senior II
  • 1251 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE 1.9.0 Tracebuffer full!

I'm running a debugee (DIYMORE STM32F407VGT6 Board) attached to SWD link adapter of a STM32F407G-DISC1 with onboard MCU disabled.I'm logging Debug messages from my C-Application using the follwoing code:while (1) { /* USER CODE BEGIN 3 */...

Debugging with Visual Studio Code

Hi, I hope to don't be off topic.Usually I use Visual Studio Code and I tried to use it for develop and debug on STM32.Unfortunately I can't debug my firmware looking at the variables in real time.I can look them only when I reach a breakpoint.With S...

SDall.11 by Associate III
  • 10654 Views
  • 6 replies
  • 0 kudos

Resolved! How do I install a newer version of CMSIS in the STMCubeIDE work environment to include PKHBT and VMAXNM/VMINNM?

I noticed that STMCubeIDE version 1.9.0 refers to a fairly old version of CMSIS V5.2.0 from May 2019 while ARM has published 5.8.0 in the meantime. Is there a way to install a newer version of CMSIS in an existing project?I have to two types of code ...

Hansel by Senior
  • 4100 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.