STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32 lwip tcp server error

I was going to make a lwip tcp server that was implemented in cube mx on cubeI get an initialization error, but I can't see it on tube mx, but it worked, so I wanted to ask how I can fix this to get rid of the errorPlease tell me howThe part where th...

ark2 by Associate III
  • 1352 Views
  • 0 replies
  • 0 kudos

remap routine in SRAM for Bootloader

Hi,I need to remap my code in SRAM for my custom Bootloader.This to be able to erase the flash dedicated to Bootloader when the Bootloader itself needs to be update.I used __attribute__ ((section(".RamFunc"))) on the functions declaration in my code....

DAUSILI by Associate III
  • 922 Views
  • 0 replies
  • 0 kudos

'Autostart local GDB Server' not working

Hi  I have been having issues in my STM32CubeIDE V1.13.1 , where the st-link couldnt be found. I finally found found the issue . In the below,  if I select  'AutoStart local GDB Server' , then I get the message 'st-link not found' . But if I run the ...

SSmit13_0-1691007623417.png

LPTIM does not count pulses from the COMP output

I want to count the pulses coming from COMP2's output using LPTIM1. However, when I send it to Tera Term, the displayed LPTIM value is consistently 1, and it doesn't match the COMP2 output.Has anyone had this problem? How did you resolve it?I would g...

Valen_id_0-1691160876385.png Valen_id_1-1691160953620.png Valen_id_2-1691160988272.png
Valen_id by Associate II
  • 6010 Views
  • 13 replies
  • 0 kudos

ADC dma without loseing samples

Hi ,i am using adc dma multibuffer mode and first buff =1000 seconf buff =1000after getting completed call back i am switching the buffer and starting multidma_buffer again but in this case i am lossing some data when i processing completed call back...

kchin.2 by Associate II
  • 2393 Views
  • 4 replies
  • 0 kudos

Impossible to rename main.c into main.cpp in sample code?

Hi,I'm using the sample HID_Standalone (USB_Host) for the board NUCLEO-H723ZG. I tried to rename the file main.c into main.cpp to force compilation with g++ instead of gcc. This worked fine with an Hello World I studied before.Unfortunately, a really...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.