STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Need help with a Cube32IDE error message

Hi Folks,I don't know what I did but the IDE is giving me a error message that I've never seen before. Here's a screen capture of the messages. It's saying that "_close is not implemented and will always fail". Is there a Project|Properties that I ne...

error_msg.JPG

Resolved! Help for my first simple bootloader STM32WLE5JC

Hi,I'm trying to create my first very simple bootloader. I'm working with Grove Wio-E5 coming from Seed with STM32WLE5JC mcu available here Important note with this mcu I don't have acces to BOOT 1 and BOOT0 very good idea coming from Seed...So my id...

SBaro.11 by Associate III
  • 2341 Views
  • 1 replies
  • 0 kudos

CubeIDE 1,8.0デバッグができない

現象午前中まで動作していましたが、急に下記の現象が発生し、デバッグができない状況です。1)ブレークポイント設定し、ブレーク後にステップイン実行ができない。 IDEからの応答がなく、停止ボタンで停止。2)ブレークポイント設定し、ブレーク後にPCレジスタ値を変更できない。 Failed to assign value 80019e0, to register 03)ブレークポイント設定し、配列データを変更すると変更した配列以外のデータが0になるMCUは、STM32H743ZI。IDEのバージョンを上...

K_I by Associate II
  • 2803 Views
  • 1 replies
  • 0 kudos

Resolved! MX_GPIO_Init' used but never defined

Here is my code and I encountered the error. I use H7A3ZI-Q board/* USER CODE BEGIN Header *//** ****************************************************************************** * @file : main.c * @brief : Main program body *****...

zniu by Associate II
  • 10571 Views
  • 6 replies
  • 2 kudos

Create a variable in SDRAM

Hi i have configured the FMC and can read and write in SDRAM extern, begin in 0xC0000000, i now want create a variable in this SDRAM, then i define:uint32_t myFrameBuffer[65280] __attribute__((section(".sdram_data"))) = {0};but when i see the debugge...

RMasi.19 by Associate II
  • 2611 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.