STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

NFC Tag Communication with M24LR04 EEROM

I have an M24LR04 NFC tag on the X-Nucleo-02A1 board connected to the Nucleo-F401RE board. I have initialized the I2C ports and other ports in STM32CubeIDE. I would like assistance writing a simple code to write some data to the M24LR04 EEROM and the...

Resolved! UART interrupt transmission or reception not happening

I am stuck dont know what i am doing is wrong ... have been stuck for 2-3 days whenever i debug it just stops (not end just that debug arrow disappears and dont move forward) after HAL_UART_Transmit_IT() in int main(). #include <stdint.h>#include "st...

Resolved! Error when building relating to .elf and flash overflow data

I did the steps below:1. Use Motor Control WorkBench to create and configure my eval board with motor characteristics with its HAL sensors2. Used CubeMX to generate the project3. Opened the generated project in CubeIDE and tried to buildI have not to...

Resolved! STM32CubeIDE Version 1.13.2 and STM32H573

Hi,I am using the STM32H573 and GCC Version 7 in CubeIDE (MS Windows) for device debugging.For debugging I am using:- STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550\tools\bin\ST-LINK_gdbserver.e...

Box69 by Associate II
  • 3186 Views
  • 4 replies
  • 0 kudos

ADC interrupt

i want to do adc sampling at 10khz frequency in stm32G070RB i have attached the ioc file configration and code but adc sampling not working at 10khz frequency. let me know where i am doing mistake and how to solve this?? 

Pooja321_0-1697796990025.png Pooja321_1-1697797051553.png Pooja321_2-1697797090073.png Pooja321_3-1697797144142.png
Pooja321 by Associate II
  • 1410 Views
  • 1 replies
  • 0 kudos

Hot to do a discovery using Device authentiction

Did numerous builds using CubeIDE (10,000 lines of code). this error started coming up. "reason was unknown target"Got the following message:Make -j4 all  DriversSTM32L4xx_HAL_Driver/subdir.mk.91:  *** unable to generate command line.  stop.  "make  ...

JBonn by Associate III
  • 1565 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.