STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

F4 Series SPI HAL Data Size Bug

I am getting a warning during compile of an incompatible pointer type when I call the SPI TransmitReceive function as shown below.Compiler warningI am passing the function an unsigned 16 bit integer array.  I have configured the SPI to use 16 data bi...

STM32CubeIDE F4 SPI_HAL compile warning.png STM32CubeMX_SPI.png STM32CubeIDE F4 SPI_HAL.png

Resolved! VERY weird 'Failed to execute MI command' problem

Hi everyone,   I start to question myself and this whole programming thing....   I'm using a STM32F3-Discovery Board and generated a code with STM32CubeMX in default mode. I changed absolutely nothing before code generation.   In main.c I added the f...

Resolved! How to import an External Tools configuration?

I have created a configuration for use of an external tool (PCLint) and successfully ran the tool in my STM IDE. I exported that configuration and got the .launch file, but now other developers on my team want to run the same external tool configurat...

AO'Do.1 by Associate
  • 4639 Views
  • 3 replies
  • 1 kudos

Resolved! IDE hangs on start - new symptom of sickness ?

This is new "option" on splash screen:!! on top: please close ioc editor --- on startup !!! Nothing is open !!-> Apply and Close --> nothing happens , just (static) splash screen.Is V1.13.1 .Only killing the java process removes the splash screen, bu...

AScha3_0-1706557490496.png AScha3_1-1706558023330.png
AScha.3 by Super User
  • 3283 Views
  • 4 replies
  • 3 kudos

Resolved! help for download this...

i need download this document of this link:https://community.st.com/t5/moderation-archive/cubeide-1-12-cyclomatic-complexity-how-it-works/td-p/71170 but after open link:You do not have sufficient privileges for this resource or its parent to perform ...

kshin.111 by Associate III
  • 1031 Views
  • 1 replies
  • 1 kudos

_Noreturn is reported as a syntax error

A syntax error is reported against the _Noreturn specified when a function is declared _Noreturn:_Noreturn void doesNotReturn( void ) { while ( 1 ) ; } The compiler has been configured for C18 and the code compiles.Can I get this to be accepted by ...

CTapp.1 by Senior III
  • 2802 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.