2025-08-06 3:00 AM
Hi,
In the bundles manager for my project is it possible to view at a glance items where there is an update available? Currently the status column icon doesn't differentiate between updatable items - only when I open the version drop-down does it become clear there are newer version(s) available (or I select all then hover over the update button).
Also, same goes for "cube pack list" command - can this show a list of updatable items?
Thanks.
Solved! Go to Solution.
2025-08-07 1:36 AM
@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.
2025-08-07 12:20 AM
Status column is right one and sortable. Variation is thin but exists. Check icon is not exactly same. One is negative of the second. Looks at it carefully.
Way to update them all thanks VSCode integrated terminal is 'cube bundle update'
I've not found way to list updatable for packs. Here way to sync. is 'cube pack sync'
2025-08-07 12:33 AM
If you look at the "System" bundles manager then yes, there is a difference in the icon, but in the project one there is not.
So here, 1.0.0 is bold and selected indicating it is the current one, but there is a newer 1.0.1 one, but the icon in the status column is indentical as far as I see.
Very minor point!
2025-08-07 1:36 AM
@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.
2025-08-18 12:00 PM
Please be aware that stm32cube-ide-bundles-manager-0.23.3.vsix has been released to address reported concerns.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.