cancel
Showing results for 
Search instead for 
Did you mean: 

Unattended installtion of STM32 Signing Tool

UVV
Associate III

According to this article the signing tool is a part of STM32CubeProgrammer. I need a signing tool during my Yocto build to be able to build signed images. The best way to guarantee a reproducibility of the build is to launch it in a dedicated container (to make sure the host system is the same on all developer / CI machines).

So the few questions are:

  1. I can't automatically download only the signing tool, can I? The download of STM32CubeProgrammer package requires for me to accept the license.
  2. It seems that STM32CubeProgrammer installer doesn't have any command line options. I would like to at least have unattended installation, automatically accepting the license and setting installation path in a non-interactive way. CubeProggrammer installation manual doesn't mention any. All that is required, for example, during 'docker build' execution.
  3. Is there an open source signing tool alternative?
1 ACCEPTED SOLUTION

Accepted Solutions
AZaki.2
Associate III

Hi @UVV ,

you can use a lightweight C++ alternative that has dependency to only OpenSSL:

https://github.com/embetrix/stm32mp-sign-tool

 

 

 

View solution in original post

1 REPLY 1
AZaki.2
Associate III

Hi @UVV ,

you can use a lightweight C++ alternative that has dependency to only OpenSSL:

https://github.com/embetrix/stm32mp-sign-tool

 

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.