2023-09-03 3:31 AM - edited 2023-09-04 1:35 AM
After building optee, tf-a and uboot the info of the fip file results in
Secure Payload BL32 (Trusted OS): offset=0x128, size=0x1C, cmdline="--tos-fw"
Secure Payload BL32 Extra1 (Trusted OS Extra1): offset=0x144, size=0x30BB8, cmdline="--tos-fw-extra1"
Non-Trusted Firmware BL33: offset=0x30CFC, size=0xF5D3C, cmdline="--nt-fw"
FW_CONFIG: offset=0x126A38, size=0x1EA, cmdline="--fw-config"
HW_CONFIG: offset=0x126C22, size=0xCFB8, cmdline="--hw-config"
and extraction of the files in
-rw-rw-r-- 1 user user 490 Sep 3 18:22 fw-config.bin
-rw-rw-r-- 1 user user 53176 Sep 3 18:22 hw-config.bin
-rw-rw-r-- 1 user user 1006908 Sep 3 18:22 nt-fw.bin
-rw-rw-r-- 1 user user 28 Sep 3 18:22 tos-fw.bin
-rw-rw-r-- 1 user user 199608 Sep 3 18:22 tos-fw-extra1.bin
The Secure Payload BL32 Extra2 (Trusted OS Extra2) seems not been added by the build scripts ? is this correct ?
BTW the pageable file are zero bytes ?
See also: https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_FIP
Solved! Go to Solution.
2023-09-15 5:53 AM
It seems when using OPTEE using page swapping on DDR BL32 extra 2 is empty. At least my boot process passes with this now.
2023-09-15 5:53 AM
It seems when using OPTEE using page swapping on DDR BL32 extra 2 is empty. At least my boot process passes with this now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.