2019-04-29 7:15 AM
Hi,
I'm trying to test the openAMP_TTY_echo from STM32Cube_FW_MP1_V1.0.1.
It compiles ok. I try the installation from : https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware#
but I fail to get the info from the "debugger" in [Upload and start the firmware].
It wants "OpenOCD Setup" but there is no info on the wiki about that.
So it loads the firmware ok but then failed with gdb/OpenOCD...
My openAMP_TTY.cfg is empty!
Thanks
Anthony Harivel
Solved! Go to Solution.
2019-04-29 7:25 AM
Hi @anthony.harivel.emtrion.GmbH
It seems you did not properly create the Debug configuration :
1 - Select the project in Project browser
2 - Right click -> Debug As .. -> Debug Configuration
3- Select "ST's STM32 MPU Debugging" - Right Click -> new
4- You should get a new Debug Target named "OpenAMP_TTY_echo Debug" containing correct information
Hope it help
Thanks to let me know
BR,
Olivier
2019-04-29 7:25 AM
Hi @anthony.harivel.emtrion.GmbH
It seems you did not properly create the Debug configuration :
1 - Select the project in Project browser
2 - Right click -> Debug As .. -> Debug Configuration
3- Select "ST's STM32 MPU Debugging" - Right Click -> new
4- You should get a new Debug Target named "OpenAMP_TTY_echo Debug" containing correct information
Hope it help
Thanks to let me know
BR,
Olivier
2019-04-30 6:43 AM
ok thanks !
I had also another issue regarding the driver of the "ST link USB dongle", but now it works !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.