2024-08-13 1:43 PM
Hello,
I am trying to boot an EMMC with a USB on a STM32MP257F-EV1 Development board and am having troubles. I set the boot pins to what is said in the data sheet for EMMC (That being Boot2 is set to 1 and the rest 0) The USB is no longer an option to connect to. (For reference I am trying to follow this wiki article: Populate the target and boot the image - stm32mpu but only using the EMMC instead of the SD Card). Any help would be greatly appreciated. Thanks!
Solved! Go to Solution.
2024-09-18 8:56 AM
Hi Erwan,
I figured out that most my problems stemmed from supplying power from the ST link and not through the Jack.
Thanks.
2024-08-14 12:28 AM
Hello @Carson ,
Can you follow this article and tell me back if you still have troubles ? https://wiki.st.com/stm32mpu/wiki/STM32MP25_Evaluation_boards_-_Starter_Package
Do not forget to connect the USB_DRD to your host PC, to verify that your CubeProgrammer is the right version (2.17) and to take the eMMC flashlayout instead of the default SDcard one.
Kind regards,
Erwan.
2024-09-18 8:56 AM
Hi Erwan,
I figured out that most my problems stemmed from supplying power from the ST link and not through the Jack.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.