2022-08-15 10:31 AM
When we tried the shutdown command ( shutdown -hP now ) from the debug console, all the PMIC regulators are turned off, except for the BUCK3 VDD regulator used for IO.
Both our custom board which uses STPMIC1E and the STM32MP157F-eval board which has STPMIC1A have the same behavior.
Is there any configuration which is not letting it to be turned off?
Any help is much appreciated.
Solved! Go to Solution.
2022-08-16 2:15 AM
Hello @SKris ,
It looks like your board is just going into standby mode. Please can you follow the best answer from this community post: https://community.st.com/s/question/0D53W00001JAWO4SAP/steps-to-lowest-power
You have to modify the DTS to allow a real system shutdown.
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-08-16 2:15 AM
Hello @SKris ,
It looks like your board is just going into standby mode. Please can you follow the best answer from this community post: https://community.st.com/s/question/0D53W00001JAWO4SAP/steps-to-lowest-power
You have to modify the DTS to allow a real system shutdown.
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-08-16 4:43 PM
Hi Kevin,
Thanks a lot for sharing the link.
The suggested changes to the tf-a device tree worked for us, now we see the buck3 being turned off when shutdown command is executed.
Thanks,
Shalini
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.