2019-07-08 11:22 PM
2019-07-09 12:07 AM
It means "Microprocessor unit", because it has no RAM and flash in it. Usually those are with Cortex-A core(s) not Cortex-M, and often is called also SoC (system on a chip).
2019-07-09 1:43 AM
But it interferes with "Memory Protection Unit", which most Cortex M devices have.
Such memory-less devices had historically been called "microprocessor".
Dunno why every vendor feels the urge to invent his own terminology.
Remember, PCMCIA.
2019-07-09 5:30 AM
The MPU boards are designed to run Embedded Linux properly, so you're building kernels, writing drivers, and apps running on the OS. I suspect they kept the things separate so as not to confuse the chaps using the MCU class devices, and those claiming to "know linux" yet have never built a kernel.
The bigger question was what fool thought calling them STM32 parts would help separate functional differences and expectations.
2019-07-10 10:58 PM
For me it is super obvious. It is not hard to guess what MPU means when the word is used alongside with MCU. It's a microprocessor that is capable of running normal Linux. And it definetely need a separate communities because it's....Linux.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.