cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257F-EV h264 decode can't work properly

mteaching
Associate III

Hello, st:

The board I have on my hand is stm32mp257f-ev1.

Now I have a problem. The gstreamer cannot work properly when playing mp4 format video.

Does the h264 decoder need to be activated or enabled?

I run this command

gst-launch-1.0 playbin3 uri="file:///home/root/Videos/2002.mp4"

here is the error:

mteaching_0-1750766157266.png

and also the gst-discovery-1.0

root@stm32mp2-e3-c2-aa:~# gst-discoverer-1.0 Videos/2002.mp4 
Analyzing file:///home/root/Videos/2002.mp4
Done discovering file:///home/root/Videos/2002.mp4
An error was encountered while discovering the file
 Failed to configure H264 decoder

It seems that I can play webm format video but not mp4.

I tried the software decode avdec_h264, but it only has 15 fps.

But in fact the h264 plugin has been installed on my board.

root@stm32mp2-e3-c2-aa:~# gst-inspect-1.0 | grep h264
codectimestamper:  h264timestamper: H.264 timestamper
libav:  avdec_h264: libav H.264 / AVC / MPEG-4 AVC / MPEG-4 part 10 decoder
rtp:  rtph264depay: RTP H264 depayloader
rtp:  rtph264pay: RTP H264 payloader
typefindfunctions: video/x-h264: h264, x264, 264
uvch264:  uvch264deviceprovider (GstDeviceProviderFactory)
uvch264:  uvch264mjpgdemux: UVC H264 MJPG Demuxer
uvch264:  uvch264src: UVC H264 Source
v4l2codecs:  v4l2slh264dec: V4L2 Stateless H.264 Video Decoder
v4l2codecs:  v4l2slh264enc: V4L2 Stateless H264 Video Encoder
videoparsersbad:  h264parse: H.264 parser

 

I just want to use gstreamer  to play a mp4 format video with the help of the hardware h264.

Do you have any suggestions?I'm looking forward your early reply.

Here is my board boot logs:

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

I got the information that today the driver of the HW video decoder inside MP25 manages video with a maximum height of 1088.

If any update occurs on the subject, I will let you know.

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
PPAGE.13
ST Employee

Hi,

to get the H264 hw accelerated decode on MP257, you need to use the following command:

"gst-launch-1.0 filesrc location=<your .mp4 file> ! qtdemux ! 
h264parse ! queue ! v4l2slh264dec ! autovideosink"

 

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello, Philippe.

I test the command you said, but still failed.

root@stm32mp2-e3-c2-aa:~# gst-launch-1.0 filesrc location=Videos/mp4/noon.mp4 ! qtdemux ! h264parse ! queue ! v4l2slh264dec ! autovideosink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Redistribute latency...
ERROR: from element /GstPipeline:pipeline0/v4l2slh264dec:v4l2slh264dec0: Failed to configure H264 decoder
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-bad/1.22.12/sys/v4l2codecs/gstv4l2codech264dec.c(334): gst_v4l2_codec_h264_dec_negotiate (): /GstPipelin:
gst_v4l2_decoder_set_sink_fmt() failed: Invalid argument
ERROR: pipeline doesn't want to preroll.
Redistribute latency...
Setting pipeline to NULL ...
Freeing pipeline ...

Now I upload the video noon.mp4 so you can also test it on your side.

BR, Bruce.

 

Hi Bruce,

I also see a problem playing any similar 720x1280 stream.
I will keep you inform of our investigation.

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi,

I got the information that today the driver of the HW video decoder inside MP25 manages video with a maximum height of 1088.

If any update occurs on the subject, I will let you know.

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello Philippe:

OK.thank you very much.

I understand now and it's normal to play the horizontal screen video.

Command

root@stm32mp2-e3-c2-aa:~# gst-discoverer-1.0 Videos/mei.mp4 
Analyzing file:///home/root/Videos/mei.mp4
Done discovering file:///home/root/Videos/mei.mp4
An error was encountered while discovering the file
 Internal data stream error.

Properties:
  Duration: 0:28:20.401000000
  Seekable: yes
  Live: no
  container #0: Quicktime
    video #1: H.264 (High Profile)
      Stream ID: 9b35559607948a0832dc591351dd1bffe2d60728bff271a52ec25e026f447dd1/001
      Width: 1280
      Height: 720
      Depth: 24
      Frame rate: 30/1
      Pixel aspect ratio: 1/1
      Interlaced: false
      Bitrate: 0
      Max bitrate: 0
    audio #2: MPEG-4 AAC
      Stream ID: 9b35559607948a0832dc591351dd1bffe2d60728bff271a52ec25e026f447dd1/002
      Language: <unknown>
      Channels: 2 (front-left, front-right)
      Sample rate: 44100
      Depth: 32
      Bitrate: 129693
      Max bitrate: 129693

 

root@stm32mp2-e3-c2-aa:~# cat test.sh 
gst-launch-1.0 filesrc location=/home/root/${1} ! qtdemux name=demux \
demux.audio_0 ! queue ! decodebin ! audioconvert ! audioresample ! autoaudiosink \
demux.video_0 ! queue ! h264parse ! v4l2slh264dec ! videoconvert ! autovideosink

 

root@stm32mp2-e3-c2-aa:~# vi test.sh 
root@stm32mp2-e3-c2-aa:~# bash test.sh Videos/mei.mp4 
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Redistribute latency...
Redistribute latency...
Redistribute latency...
Redistribute latency...0.0 %)
Redistribute latency...0.0 %)
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
Redistribute latency...
New clock: GstPulseSinkClock
Redistribute latency...0.0 %)

BR

Bruce.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.