2023-07-26 2:42 AM
Hello, I've just migrated from V4.1.0 dev package to V5.0.0 and the LCD SPI ilitek 9486 does not work anymore.
Configuration: STM32MP157A-DK1 with 3.5 LCD SPI touchscreen. Starter Package loaded with stm32mp157c-dk2 config. Linux kernel recompiled with ili9486 module and uploaded. Device tree file "stm32mp157c-dk2.dts" modified with spi5 added and display and uploaded.
Please, how can I do to recover the LCD SPI that worked on previsous dev package?
2023-07-26 4:58 AM
Hi @remyguerry ,
Thanks to raise this point to us.
Can you please elaborate a bit how you migrate from DV4.1 to DV5.0 ?
Did you start from scratch and use MX to generate updated DT ?
Did you update on board BSP + Kernel ?
Any boot log from working DV4.1 and not working DV5.0 you may share ?
Thanks
Olivier
2023-07-26 6:17 AM
Hi Olivier,
Thank you for quick response.
It is not really a migration, I've followed steps from scratch in command line with new working directory DV5.0.
Please find bootlogs to see differences.
Thanks,
Remy
2023-07-26 6:18 AM
Checking your DTS it can be noticed :
- no status = "okay" in spi5 node
- double dsi_in declaration in both spi5 and dsi node
both may explained issue.
Olivier
2023-07-26 6:24 AM
Hi @remyguerry ,
If your step 3 is to reuse 4.1 dts as it in DV5 I'm afraid it could be root cause of many issues.
Some Policies and device tree architecture may have slightly change between both version.
It could be worth to rather copy/paste ONLY your change in dts 4.1 into dts 5.0 ...
Olivier
2023-07-26 6:33 AM
I think status = "okay" there is. Do I have to put under display:display@0 node also?
dsi node is commented, I will declare another name to be sure.
Thanks.
Remy
2023-07-26 6:38 AM
In step 3, I've just copy/paste changes as your advice. Sorry for missing this precision.
2023-10-06 2:59 AM
Hi @Olivier GALLIEN ,
I went further in the subject and found there is an error with mapping of PRIME buffer.
The LCD shows OpenST linux picture the first time I upload new kernel compilation, just before doing "sbin/depmod -a sync reboot". But after the reboot I have the error "Failed to vmap PRIME buffer" and nothing on LCD display. The error comes from ili9486.c driver were there are some little changes from DV4.1 to DV5.0. Can I do something in DTS or somewhere for PRIME buffer mapping?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.