2019-06-26 11:00 AM
UART7 is not working when configured with same pin numbers as given in the STMCubeMX code.
When connected as per schematic pin config, it is working.(Corresponding code also changed)
So why is this happening like this?
Please help.
Solved! Go to Solution.
2019-06-27 1:11 AM
Hello,
STM32CubeMX setup for STM32MP157C-DK2 board does not automatically allocate Arduino peripherals on right location (as not used in our Starter Package demo and Arduino pins could be used for many usages). Simply activating UART7 make CubeMx to assign RX/TX to a free ball, without guarantee it is the one corresponding on the board schematics.
Under CubeMx, you have to assign manually the UART7_TX/RX on PE8/PE7 respectively:
2019-06-27 1:11 AM
Hello,
STM32CubeMX setup for STM32MP157C-DK2 board does not automatically allocate Arduino peripherals on right location (as not used in our Starter Package demo and Arduino pins could be used for many usages). Simply activating UART7 make CubeMx to assign RX/TX to a free ball, without guarantee it is the one corresponding on the board schematics.
Under CubeMx, you have to assign manually the UART7_TX/RX on PE8/PE7 respectively:
2019-06-27 1:29 AM
Hello Patrick,
Thank you for the clarification.
We have a more important problem in the same area. Combination of OpenAMP framework and UART7.
I created a separate question for that.
This is very important for us. Please clarify.
Thank you.
Best Regards,
Upendar Reddy Sama
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.