2024-08-05 11:27 PM
Kernel tree does not assign any driver to pin PZ2. After gpioset -c gpiochip11 2=1, the pins goes actually high (from low) but the gpioset program stalls. SSH at that moment into the device shows:
line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" output consumer="gpioset"
line 3: "PZ3" input
line 4: "PZ4" input consumer="kernel"
line 5: "PZ5" input consumer="kernel"
line 6: "PZ6" input
line 7: "PZ7" input
Aborting CTRL-C/Z gpioset causes the device to be busy upon a next set.
Is there a way to set the pin and the client release itself as consumer of GPIO pin to be able to change the pin later back to low?
root@stm32mp1:~# gpioset -c gpiochip11 2=1
^Z[1]+ Stopped gpioset -c gpiochip11 2=1
root@stm32mp1:~# gpioset -c gpiochip11 2=0
gpioset: unable to request lines on chip '/dev/gpiochip11': Device or resource busy
root@stm32mp1:~# gpioget -c gpiochip11 2
gpioget: unable to request lines: Device or resource busy
Solved! Go to Solution.
2024-08-06 2:02 AM
Hi @debugging
according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.
To force exit of gpioset immediately, you need to use '-t0'
gpioset -t0 -c gpiochip11 2=1
Regards.
2024-08-06 2:02 AM
Hi @debugging
according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.
To force exit of gpioset immediately, you need to use '-t0'
gpioset -t0 -c gpiochip11 2=1
Regards.
2024-08-07 1:07 AM - edited 2024-08-07 1:07 AM
Tank you very much. this helps a lot. Perhaps good to add to the wiki.
2024-08-07 1:26 AM
wiki update is planned even if the listed CTRL+C works and this is more a libgpio v2 specificity (seems an intended behavior).
I think it is minor as only command line issue. In an application, behavior is more clean.
regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.