cancel
Showing results for 
Search instead for 
Did you mean: 

SMT32MP15 ECO 5.0 Can't enable backlight PWM timer 2 channel 1

debugging
Lead

An simple RGB LCD panel does not show any screen or backlight.

Trying to solve that to enable the PWM backlight timer for it.

Some post followed:

https://www.kernel.org/doc/Documentation/devicetree/bindings/display/st%2Cstm32-ltdc.txt
https://community.st.com/t5/stm32-mpus-products/how-to-add-pwm-backlight-to-timer-block/td-p/213372
https://community.st.com/t5/stm32-mpus-embedded-software/pwm-backlight-not-working-can-you-please-check-my-device-tree/td-p/202199
https://community.st.com/t5/stm32-mpus-embedded-software/how-to-use-timers2-as-pwm-backlight/td-p/357071

cat /sys/kernel/debug/pinctrl/soc\:pinctrl@50002000/pinconf-pins | grep PA5
pin 5 (PA5): alternate 1 (TIM2_CH1 TIM2_ETR) - push pull - pull down - low speed

root@stm32mp1:~# cat /sys/kernel/debug/pwm

 

 

 

platform/40000000.timer:pwm, 4 PWM devices
pwm-0 (backlight ‌ requested enabled period: 5000000 ns duty: 5000000 ns polarity: normal
pwm-1 ((null) ‌ period: 0 ns duty: 0 ns polarity: normal
pwm-2 ((null) ‌ period: 0 ns duty: 0 ns polarity: normal
pwm-3 ((null) ‌ period: 0 ns duty: 0 ns polarity: normal

 

 

 

root@stm32mp1:/sys/class/pwm# ls -l

 

 

 

lrwxrwxrwx 1 root root 0 Aug 9 09:58 pwmchip0 -> ../../devices/platform/soc/5c007000.etzpc/40000000.timer/40000000.timer:pwm/pwm/pwmchip0

 

 

 

 

cd /sys/class/pwm/pwmchip0  (timer 1)

# select channel 1

echo 0 > export

sh: write error: Device or resource busy

DTS:

 

 

 

&timers2 {
status = "okay";
/* spare dmas for other usage */
/delete-property/dmas;
/delete-property/dma-names;
counter {
status = "okay";
};
pwm2: pwm {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pwm2_pins_b>;
pinctrl-1 = <&pwm2_sleep_pins_b>;
#pwm-cells = <2>;
status = "okay";
};
timer@1 {
status = "disabled";
};
};

 

 

 

after a reboot (p.s none of values worked, from 0 ... n

 

 

 

root@stm32mp1:/sys/class/pwm/pwmchip0# echo 1 > unexport
root@stm32mp1:/sys/class/pwm/pwmchip0# echo 1 > export
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm1# cat enable
0
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm1# echo 10000 > period
sh: write error: Device or resource busy
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm1# echo 10000 > duty_cycle
sh: write error: Invalid argument

 

 

 

not enabled, but busy ?

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
debugging
Lead

Backlight did work, Issue  was caused by a LCD pin keeping LCD backlight/PWM regulators disabled.

View solution in original post

1 REPLY 1
debugging
Lead

Backlight did work, Issue  was caused by a LCD pin keeping LCD backlight/PWM regulators disabled.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.