2021-12-03 5:52 AM
Hello.
I developed my own board based on A-DK1 board using STM32MP157CAC and MicroSD, PMIC, Ethernet and DDR periphery. When I connect my plate to the usb with sd-card (st-link 2.1) I always receive the message:
PANIC at PC : 0x2fff2d17
Exception mode=0x00000016 at: 0x2fff2d17
Only these 2 strings.
My power and clock schematics exactly the same as -dk1 board.
I have only one difference. There is a STM32MP157AAC on the dk-1 and I use STM32MP157CAC...I have one sd-card for the both boards. My MPU just doesn't wake up and I don't understand what should I doing
Solved! Go to Solution.
2021-12-03 6:22 AM
Hi,
may I suggest you to check for classic pitfall/debug steps:
https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure
Going from STM32MP157A to STM32MP157C should not be the root cause of your issue.
By experience, one of the first frequent pitfall is using an HSE Crystal with a Device Tree set for HSE bypass (BootROM has autodetect, but TF-A used Device Tree settings)
Then once first verification steps are not solving your issue, please share the Device Tree you used to compile your SD-Card binaries and the complete TF-A log.
Note that I wonder if the Starter Package SD-Card of STM32MP157A-DK1 will work on a custom board (as in Starter Package there is probably some automated board detection based on custom OTPs sets only on ST development boards).
Btw, I will put your precedent ticket as 'answered'
Regards,
Patrick
2021-12-03 6:22 AM
Hi,
may I suggest you to check for classic pitfall/debug steps:
https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure
Going from STM32MP157A to STM32MP157C should not be the root cause of your issue.
By experience, one of the first frequent pitfall is using an HSE Crystal with a Device Tree set for HSE bypass (BootROM has autodetect, but TF-A used Device Tree settings)
Then once first verification steps are not solving your issue, please share the Device Tree you used to compile your SD-Card binaries and the complete TF-A log.
Note that I wonder if the Starter Package SD-Card of STM32MP157A-DK1 will work on a custom board (as in Starter Package there is probably some automated board detection based on custom OTPs sets only on ST development boards).
Btw, I will put your precedent ticket as 'answered'
Regards,
Patrick
2021-12-07 3:44 AM
Thank you very much! I had a mistake in my I2C4 schematic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.