cancel
Showing results for 
Search instead for 
Did you mean: 

OP-TEE Trusted Application examples fail to run on STM32MP157F-DK2

Pavestone7762
Associate II

I'm attempting to run an OP-TEE Trusted Application on the STM32MP157F-DK2 running OpenST Linux version stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21. I've followed the guides here and here, but both end up producing the following error when attempting to run the application:

TEEC_Opensession failed with code 0xffff0008 origin 0x3

What could be causing this problem? I'm running a fresh install of OpenST Linux and haven't made any modifications to the system other than those required to get the example running.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavestone7762
Associate II

I found on this page that OP-TEE user trusted applications are disabled by default for ecosystem release v5.0.0. (It would have been helpful for this to be documented on this page as well...)

View solution in original post

1 REPLY 1
Pavestone7762
Associate II

I found on this page that OP-TEE user trusted applications are disabled by default for ecosystem release v5.0.0. (It would have been helpful for this to be documented on this page as well...)