2021-09-02 4:18 AM
Hi,
I have a STM32MP157a-dk1 discovery board and a SX 1280 – Semtech (E28 2G4M27S - E-Byte) module.
With CubeMX I add SPI5 to the architecture and get the outputs (Kernel, TF-A and U-boot files.) Then by using these output files I can generate the DTB file and can flash this at DK1 card side.
Below SPI loopback test is OK also.
https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev
What I want to learn is:
Actually, I am very new to Embedded Linux concept. I don't even know what is the structure of
driver. But as I see I need to apply my SX 1280 Lora IC's communication specs to STM32MP1 series MPU side.
Can any one offer me where to start?
As you can see I am thinking to use MPU side of the IC. Maybe MCU side can also be used as well.
I want to get data from ethernet then need to send this data over SX 1280.
2021-09-02 11:26 PM
Hi again,
For me this question is really important. Can you please check if my decision is right or has gaps and errors?
Sincerely, thanks..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.