2021-03-13 3:26 AM
We use HSE osc instead of xtal as suggested by errata. However to support STANDBY we need to turn it off by GPIO. The idea is to boot from SPINAND on HSI and turn HSE in bootloader.
Unfortunately it seems that ROM hangs when HSE is not present:
< @ 00646143 | [INFO] - BOOTCORE_Pll1Started >
< @ 00651111 | [INFO] - BOOTCORE_Pll1Locked >
< @ 00652481 | [INFO] - BOOTCORE_Pll2Started >
< @ 00657398 | [INFO] - BOOTCORE_Pll2Locked >
< @ 00658999 | [INFO] - BOOTCORE_CkMpuSsSwitchedOnPll1 >
< @ 00660470 | [INFO] - BOOTCORE_CkAxiSsSwitchedOnPll2 >
< @ 00661050 | [INFO] - BOOTCORE_Pll12StartReqStatusPllStarted >
< @ 00824184 | [INFO] - NANDCORE_GetParamFromOtp >
< @ 05653430 | [INFO] - BOOTCORE_HseNoBypass >
< @ 06934011 | [ERR ] - BOOTCORE_HseNotReady >
I tried to set CFG9 bits 1 and 2 (skip HSE detects) but no success. Setting bit 5 in CFG3 (skip PLLs) doesn't help too.
Is HSE usage somehow hardcoded for SPINAND boot ? From docs I get that only USB needs HSE...
thanks, Martin
Solved! Go to Solution.
2021-03-13 4:24 AM
Oops, disregard the post please.
I found bad flash populated ( W25N01GWxxIT instead if xxIG) which has "continuous mode read" feature default on. So that it work after soft reboot because my bootloader turns the feat off. But cold boot fails. New HSE circuit on the same board was only coincidence.
M.
2021-03-13 4:24 AM
Oops, disregard the post please.
I found bad flash populated ( W25N01GWxxIT instead if xxIG) which has "continuous mode read" feature default on. So that it work after soft reboot because my bootloader turns the feat off. But cold boot fails. New HSE circuit on the same board was only coincidence.
M.
2021-03-15 2:15 AM
Hi,
Good to see you find the root cause.
I confirm that the :
< @ 06934011 | [ERR ] - BOOTCORE_HseNotReady >
Was due to BootROM fallback to Serial/USB boot due to issue with the Flash content/access.
Btw, to ease analysis, it is always better to provide full BootROM Trace (which is usually small and does not contain sensitive information)
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.