2019-06-27 2:49 AM
There's some inconsistency on the support of LPDDR2/3 on LFBGA448/LFBGA354 package.
Page 16 of the datasheet lists that LPDDR is only supported on TFBGA257/361, which is consistent with the settings in CubeMX (LFBG* packages have on LPDDR option).
However, page 10 & 11 of AN5122 STM32MP1 Series DDR memory routing guidelines clearly show that LPDDR is supported on both LFBGA packages.
I guess this is an error in the datasheet and CubeMX?
2019-07-01 5:58 PM
As I'm finalizing the part selection for a STM32MP1 based design, any comment on this issue would be much appreciated!
Shenshen
2019-07-29 4:36 AM
Did you got some information regarding this ? We have the same problem...
Martin
2019-07-29 11:09 AM
No, I haven't heard anything from ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.