2021-07-16 2:11 AM
I am looking for STM32MP157A-DK1 and STM32MP157A-DK2 Why thouse boards is not recommended for new design? Which developer board you can recommend?
@PatrickF @Community member @SEam72
Solved! Go to Solution.
2021-07-16 2:28 AM
Hi,
These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).
STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2
Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)
Regards.
2021-07-16 2:28 AM
Hi,
These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).
STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2
Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)
Regards.
2021-07-16 2:30 AM
You can use the successor boards STM32MP157D-DK1 and STM32MP157F-DK2.
Good luck!
/Peter
2021-07-16 2:39 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.