2025-04-10 6:57 AM
Hello,
I use STM32MP1 SoC. According to wiki I can interrupt uploading images with STM32 Cube Programmer via USB-DFU: For USB boot, you can easily interrupt this command stm32prog usb 0by pressing Ctr + C in the console without U-Boot modification.
U-boot also prints in its console "Ctrl+C to exit", but in fact I cannot send "Ctrl+C". It looks like U-boot console is read-only while uploading via USB-DFU. What is wrong ?
At normal boot (from eMMC), I can interrupt U-boot loading and use console perfectly. I use minicom for U-boot console
2025-04-14 1:53 AM
Hi,
the U-Boot console is deactivated only for serial boot over UART.
But for serial boot over USB, the U-Boot console is functional (read and write), and the reception of the Ctrl^C in the console is handled in the DFU loop to interrupt the pending request.
see => source/common/dfu..::run_usb_dnl_gadget()
if (ctrlc()) goto exit;
Your issue is perhaps linked to management of special character for the used tools for console: minicom.
For normal boot, the boot command is interruption by any key pressed, Ctrl^C is not required. But it is required to interrupt the DFU command.
On my side I use picocom on Linux on avoid some strange side effect of minicom (as this tools was designed for communication with modem).
Can you try with a more simple terminal tool?
Patrick
2025-04-15 7:47 AM
I tried using picocom without success.
While normal boot I can write into U-boot console. For instance, if I boot from eMMC and press Ctrl+C I get this string in U-boot:
STM32MP> <INTERRUPT>
While uploading images via USB-DFU with STM Cube Programmer I get the prompt
UPLOAD ... done
Ctrl+C to exit ...
But Ctrl+C still does not work, U-boot console seems read-only.
Moreover, when I try to boot from SD card without SD card, I get U-boot prompt
Card did not respond to voltage select!
mmc_init: -95, time 12
STM32MP>
but I cannot enter commands neither
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.