2022-12-01 11:26 PM
Hi,
I was downloading and installing Distribution package for the 1st time following this link: https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/STM32MP1_Distribution_Package
As I want version openstlinux-5.10-dunfell-mp1-21-03-31
After source sync there are no files present. May I know why its discarding?
root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.10-dunfell-mp1-21-03-31
.repo/manifests/: discarding 3 commits
Your identity is: ***.*** [removed by moderator]
If you want to change this, please re-run 'repo init' with --config-name
Testing colorized output (for 'repo diff', 'repo status'):
black red green yellow blue magenta cyan white
bold dim ul reverse
Enable color display in this user account (y/N)?
repo has been initialized in /
If this is not the directory in which you want to initialize repo, please run:
rm -r //.repo
and try again.
root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo sync
Fetching project openembedded-core
Fetching projects: 12% (1/8)
Fetching project meta-openembedded
Fetching projects: 25% (2/8)
Fetching project bitbake
Fetching projects: 37% (3/8)
Fetching project meta-st-openstlinux
Fetching projects: 50% (4/8)
Fetching project meta-st-stm32mp
Fetching projects: 62% (5/8)
Fetching project meta-qt5/meta-qt5
Fetching projects: 75% (6/8)
Fetching project meta-st-scripts
Fetching projects: 87% (7/8)
Fetching project meta-st-stm32mp-addons
Fetching projects: 100% (8/8)
Fetching projects: 100% (8/8), done.
Syncing work tree: 100% (8/8), done.
layers/meta-openembedded/: discarding 137 commits
layers/meta-qt5/: discarding 6 commits
layers/meta-st/meta-st-openstlinux/: discarding 24 commits
layers/meta-st/meta-st-stm32mp/: discarding 36 commits
layers/meta-st/meta-st-stm32mp-addons/: discarding 4 commits
layers/meta-st/scripts/: discarding 2 commits
layers/openembedded-core/: discarding 587 commits
layers/openembedded-core/bitbake/: discarding 23 commits
root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# ls
root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31#
Thankyou
2022-12-20 6:49 AM
Hello,
I recommend you to use the latest version of the distribution package.
Regards,
Grégory
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.