2019-12-18 10:25 PM
2019-12-24 1:38 AM
when you choose one of the SPIs, say for example, SPI1, some of the pins are selected as TX, RX and CLK, standing for transmitter, receiver, and clock pins. you can receive the data on the RX pin. the relevant HAL function would be HAL_SPI_Receive().
2019-12-24 1:44 AM
BSP_LED_Off(LED2);
HAL_SPI_Transmit(&SpiHandle,&adres,1,HAL_MAX_DELAY);
HAL_SPI_Receive(&SpiHandle,&data,1,HAL_MAX_DELAY);
BSP_LED_On(LED2);
That's part of my code. Sending data via transmit I want to read the data sent by the receiver but it shows 0.
2019-12-24 2:23 AM
are you sure that "data" contains anything? because in the above code I can see nothing... have you initialized "data"?
2019-12-24 6:11 AM
#include "main.h"
#define MASTER_BOARD
SPI_HandleTypeDef SpiHandle;
uint8_t aTxBuffer = 0x55;
uint8_t aRxBuffer;
void SystemClock_Config(void);
static void Error_Handler(void);
void spi_Init(void);
//static uint16_t Buffercmp(uint8_t *pBuffer1, uint8_t *pBuffer2, uint16_t BufferLength);
int main(void)
{
HAL_Init();
SystemClock_Config();
spi_Init();
BSP_LED_Init(LED2);
// CS5532_Init();
#ifdef MASTER_BOARD
SpiHandle.Init.Mode = SPI_MODE_MASTER;
#else
SpiHandle.Init.Mode = SPI_MODE_SLAVE;
#endif
if(HAL_SPI_Init(&SpiHandle) != HAL_OK)
{
Error_Handler();
}
/*
#ifdef MASTER_BOARD
BSP_PB_Init(BUTTON_USER, BUTTON_MODE_GPIO);
while (BSP_PB_GetState(BUTTON_USER) != GPIO_PIN_RESET)
{
BSP_LED_Toggle(LED2);
HAL_Delay(100);
}
BSP_LED_Off(LED2);
#endif */
HAL_SPI_Transmit(&SpiHandle, &aTxBuffer,1, 5000);
HAL_SPI_Receive(&SpiHandle,&aRxBuffer,1, 5000);
HAL_Delay(1);
BSP_LED_Off(LED2);
while (1)
{
}
}
static void Error_Handler(void)
{
while(1)
{
BSP_LED_Toggle(LED2);
HAL_Delay(1000);
}
}
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
/* MSI is enabled after System reset, activate PLL with MSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 40;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLP = 7;
RCC_OscInitStruct.PLL.PLLQ = 4;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
while(1);
}
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
while(1);
}
}
void spi_Init(void)
{
SpiHandle.Instance = SPIx;
SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;
SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW;
SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE;
SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle.Init.CRCPolynomial = 7;
SpiHandle.Init.CRCLength = SPI_CRC_LENGTH_8BIT;
SpiHandle.Init.NSS = SPI_NSS_SOFT;
SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
}
/*static uint16_t Buffercmp(uint8_t* pBuffer1, uint8_t* pBuffer2, uint16_t BufferLength)
{
while (BufferLength--)
{
if((*pBuffer1) != *pBuffer2)
{
return BufferLength;
}
pBuffer1++;
pBuffer2++;
}
return 0;
} */
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
while (1)
{
}
}
#endif
my full code is as follows. can you help
2019-12-24 9:37 AM
Which STM32 part are we talking about?
I think if you want two way comms you'd do better using the Transmit_Receive function.
You'd also want to consider how you're driving the chip-select into the unspecified target device.
2019-12-24 9:22 PM
I use the STM32 l476 card. Cs5532 I want to get information from ADC. For this, I first tried to communicate between 2 stm32. I wonder why the Receive function doesn't work.
2019-12-24 10:53 PM
safe SPI is 4 wires MOSI/MISO/SCK/NSS
receive and transmit occur at the same time so you need to use transmit_receive
There are (too) simple examples in Nucleo project folders... to help you get started.
2019-12-24 11:24 PM
Only transmitreceive is used in the examples I could not see the example related to Receive
2019-12-25 10:46 AM
Still use transmit receive, even if you don't configure all SPI GPIOs.]
All works fine with STM32L496 SPI master and slave modes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.