2022-03-09 4:49 PM
I want to use sysinitv instead of systemd . When I add DISTRO_FEATURES_remove = "systemd" in Distro conf ,bitbake stopped whit ERROR: /home/st/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-openembedded/meta-initramfs/recipes-core/packagegroups/packagegroup-meta-initramfs.bb: Please ensure that your setting of VIRTUAL-RUNTIME_init_manager (systemd) matches the entries enabled in DISTRO_FEATURES
ERROR: Failed to parse recipe: /home/st/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-openembedded/meta-initramfs/recipes-core/packagegroups/packagegroup-meta-initramfs.bb
Solved! Go to Solution.
2022-03-15 3:21 AM
Hello @Yby.1
Please, from your main source folder, go to: layers/openembedded-core/meta/conf/distro/
In this folder you will find a file named defaultsetup.conf.
This file contains the following line :
INIT_MANAGER ??= "none"
What happens here is that, if you do not define another thing instead of none, Yocto will take systemd as Init Manager by default. However you can replace this "none" by "sysvinit".
If you do that, Yocto will include variables presents in ./include/init-manager-sysvinit.inc
content :
# Use sysvinit for system initialization
DISTRO_FEATURES_append = " sysvinit"
DISTRO_FEATURES_BACKFILL_CONSIDERED_append = " systemd"
VIRTUAL-RUNTIME_init_manager ??= "sysvinit"
VIRTUAL-RUNTIME_initscripts ??= "initscripts"
VIRTUAL-RUNTIME_login_manager ??= "busybox"
Of course you can define these variables in you local.conf file to compile with Bitbake if you prefer. This is just another way to do it.
Hope this information will help you.
Regards.
Erwan.
2022-03-15 3:21 AM
Hello @Yby.1
Please, from your main source folder, go to: layers/openembedded-core/meta/conf/distro/
In this folder you will find a file named defaultsetup.conf.
This file contains the following line :
INIT_MANAGER ??= "none"
What happens here is that, if you do not define another thing instead of none, Yocto will take systemd as Init Manager by default. However you can replace this "none" by "sysvinit".
If you do that, Yocto will include variables presents in ./include/init-manager-sysvinit.inc
content :
# Use sysvinit for system initialization
DISTRO_FEATURES_append = " sysvinit"
DISTRO_FEATURES_BACKFILL_CONSIDERED_append = " systemd"
VIRTUAL-RUNTIME_init_manager ??= "sysvinit"
VIRTUAL-RUNTIME_initscripts ??= "initscripts"
VIRTUAL-RUNTIME_login_manager ??= "busybox"
Of course you can define these variables in you local.conf file to compile with Bitbake if you prefer. This is just another way to do it.
Hope this information will help you.
Regards.
Erwan.
2023-03-01 8:56 AM
Awesome!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.