2019-08-20 11:47 PM
Hi,
I want to compile linux kernel for stm32mp157c-dk2, i followed guide in README.HOW_TO.txt and when i run command "make ARCH=arm O="$PWD/../build" multi_v7_defconfig fragment*.config" in point 5. I get following errors:
/opt/st/stm32mp1/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9/scripts/kconfig/Makefile:109: *** No configuration exists for this target on this architecture. Stop.
/opt/st/stm32mp1/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9/Makefile:539: recipe for target 'fragment*.config' failed
make[2]: *** [fragment*.config] Error 2
/opt/st/stm32mp1/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9/Makefile:286: recipe for target '__build_one_by_one' failed
make[1]: *** [__build_one_by_one] Error 2
make[1]: Opuszczenie katalogu '/opt/st/stm32mp1/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/build'
Makefile:146: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
I did everything before without point 4 (cuz i think it is optional) and without applying patches in point 3. because i don't know where to find this patches.
Besides this errors, some files are generated in ../build directory. Including .config and i am able to compile kernel, but when i deploy it on board, system crashes. And i think thats because of this previous errors.
Please tell me what I am doing wrong and how can i make it work
Solved! Go to Solution.
2019-08-21 2:08 AM
Hi @La
README.HOW_TO.txt procedure has been carefully validated/tested and works.
If you have properly source the SDK environnement step 2, I guess problem come from the fact you drop step 3.
Patches are present in folder sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0
So command to apply from sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9 is :
for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Hope it help
Olivier
2019-08-21 2:08 AM
Hi @La
README.HOW_TO.txt procedure has been carefully validated/tested and works.
If you have properly source the SDK environnement step 2, I guess problem come from the fact you drop step 3.
Patches are present in folder sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0
So command to apply from sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9 is :
for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Hope it help
Olivier
2019-08-21 3:41 AM
Thanks so much ! Everything now works :)
2020-12-04 5:13 AM
Hello I got the same issue but when I go to the patch directory and I do
for p in `ls -1 ../*.patch`; do patch -p1 < $p; donecannot access '../*.patch': No such file or directory
2020-12-07 12:40 AM
You need to be in sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9 directory, not in patch directory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.