2024-12-27 3:00 PM
Hello,
I have tried following the https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_OTP_management to achieve this.
I have tried configuring
CFG_BSEC_PTA=y CFG_STM32_BSEC_WRITE=y CFG_WITH_USER_TA=y
into the meta-st-stm32mp bsp and verified that it was being added to the make.
I then did a minimal flashlayout to get to uboot. I have tried multiple setting/configs but I always get the same error when i run the command; STM32_Programmer_CLI -c port=usb1 -otp displ
optee optee: TA_NVMEM invoke failed TEE err: ffff0006, err:0
Error: OTP read issue -5
dfu_read: Failed to fill buffer
What is the one thing that I am missing here? My goal is to be able to flash word 3, 5, & 6. Any help would be appreciated, thank you.
Solved! Go to Solution.
2025-05-14 9:41 AM
Hi,
Maybe try this lightweight alternative
https://wiki.st.com/stm32mpu/wiki/STM32PRGFW-UTIL
https://github.com/STMicroelectronics/STM32PRGFW-UTIL/blob/main/README.md
Regards.
2025-05-13 7:36 AM
Hi, were you able to figure this out? I'm seeing this problem as well.
2025-05-13 8:36 AM
Check if the UUID for the NVMEM TA in OP-TEE matches the one expected by the STM32_Programmer_CLI. If the UUIDs don’t match, the invocation will fail.
Check the UUID in your OP-TEE TA source (or in ta/arm-plat-stm32mp1/nvmem/uuid.c) and compare with what the STM32_Programmer_CLI expects.
2025-05-14 9:41 AM
Hi,
Maybe try this lightweight alternative
https://wiki.st.com/stm32mpu/wiki/STM32PRGFW-UTIL
https://github.com/STMicroelectronics/STM32PRGFW-UTIL/blob/main/README.md
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.