2021-06-03 3:36 AM
Hi everyone,
I'm interested how can someone backup rootfs, vendorfs etc and later use that to flash via the STM32CubeProgrammer? Is using the dd good way to do it?
Best regards,
Nenad
2021-06-09 6:27 AM
Hi NGajic (Community Member)
You can certainly backup ext4 partitions or the entire image to another flash after mounting it (SDcard/USB dongle). I would use dd as it is straightforward. Then flash the partition back for later use using STM32CubeProgrammer.
If you have an SDcard reader, it is a no brainer job. Otherwise use the board USB mass storage feature in u-boot (in a boot console), ums 0 mmc 0 if you have USB connected (usb OTG on DK2 board)
Best Regards,
Olivier
2021-06-10 5:43 AM
Hi,
maybe some help on this page: https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
which is describing the reverse way (from local binaries to SD image), but I think analyzing the script could bring information how to do the reverse (from SD image to local binaries).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.