2022-07-25 9:23 AM - last edited on 2023-06-16 9:16 AM by Kevin HUBER
From instructions, I opened two console:
Console 1: openocd -f board/stm32mp15x_dk2.cfg
This looks good as output:
```
...
Info : stm32mp15x.cm4: Cortex-M4 r0p1 processor detected
Info : stm32mp15x.cm4: target has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu0 rev 5, partnum c07, arch f, variant 0, implementor 41
Info : stm32mp15x.cpu0: MPIDR level2 0, cluster 0, core 0, multi core, no SMT
Info : stm32mp15x.cm4: external reset detected
Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu1 rev 5, partnum c07, arch f, variant 0, implementor 41
Info : stm32mp15x.cpu1: MPIDR level2 0, cluster 0, core 1, multi core, no SMT
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for stm32mp15x.cpu0 on 3333
Info : Listening on port 3333 for gdb connections
Info : starting gdb server for stm32mp15x.cm4 on 3334
Info : Listening on port 3334 for gdb connections
```
Console 2:
gdbgui -g "arm-ostl-linux-gnueabi-gdb -x gdb-script/Setup.gdb"
gdb-script folder is in same location where I run run command.
If I don't pass '-p 3333' then default is 127.0.0.1:5000 and failed.
If I add -p 3333 then:
OSError: [Errno 98] Address already in use
I already reset computer to "kill the gdbgui instance running in background" but did not help!
Anyone know how fix this issue?
And, the port is 5000 or 3333 if I want to debug over ST link?
edit:
Look to me port 3333 is right one. When look at console 1 where openocd start, I see:
```
Info : New GDB Connection: 1, Target stm32mp15x.cpu0, state: halted
Warn : ignoring character 0x47
Warn : ignoring character 0x45
.....
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1016 ms). Workaround: increase "set remotetimeout" in GDB
```
When use port 5000 nothing happen at all.
Still see "OSError: [Errno 98] Address already in use" from gdbgui console if use port 3333
2022-07-26 8:41 AM
Hi Dat Tran (Community Member),
port 3333 is indeed the correct one to use
Open On-Chip Debugger 0.11.0-rc2-dirty (2021-10-29-14:02)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J36M26 (API v2) VID:PID 0483:3752
Info : Target voltage: 3.259064
Info : Unable to match requested speed 5000 kHz, using 4000 kHz
Info : Unable to match requested speed 5000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stm32mp15x.cm4: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cm4: external reset detected
Info : starting gdb server for stm32mp15x.cpu0 on 3333
Info : Listening on port 3333 for gdb connections
Info : starting gdb server for stm32mp15x.cm4 on 3334
Info : Listening on port 3334 for gdb connections
2022-07-26 9:36 AM
Yes, I will focus only on port 3333 from now.
But when Openocd listen at port 3333
And gdbgui also listen at port 3333,
This causes another error: "Address already in use", and I read python source code, "SO_REUSEADDR" already set before bind socket.
Do you have any idea?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.