2019-05-21 3:27 AM
Hello,
I'm currently working into STM32MP157C-DK2 and I have made my own image with the following append:
apache2 php phpmyadmin php-cli mysql5
But into my internet page (move from //usr/share/.. to another directory) php code didn't work and when I try to configure mysql5 I have this
ERROR 2002 (HY000): Can't connect to local MySQL server through socket '/var/lib/mysql/mysql.sock' (2)
Also I try to add php-modphp but the bitbake fail
I try too to install dev-pkgs but I get an error too
Do you have any idea ?
2019-06-24 9:03 AM
Hi @AZAMA
Sorry for late reply.
Is this post still valid ?
Most of the module you mentioned are by default integrated to the default OpenSTLinux running on DK2 through meta-oe and meta-webserver layers.
Could then please be more specific on what you have done to generate your own image and share the logs in case of errors.
Thx
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.