2019-07-19 3:07 PM
I would like to understand what the Eclipse IDE is doing to start the debugger, so that I can move away from using it. I much prefer CMake and other tools. I'd be grateful for any assistance. The wiki section for this is TBD.
I'm not too familiar with OpenOCD, but have run the command:
$OECORE_NATIVE_SYSROOT/usr/bin/openocd -s $OECORE_NATIVE_SYSROOT/usr/share/scripts -f board/stm32mp15x_dk2.cfg
This seems to work so, moving on to GDB:
$OECORE_NATIVE_SYSROOT/usr/bin/arm-openstlinux_weston-linux-gnueabi/arm-openstlinux_weston-linux-gnueabi-gdb firmware.elf
And this is where I come unstuck. I've used GDB a bit, but don't know the magic incantations to install an image into the M4 on this platform.
(gdb) target remote localhost:3333
Remote debugging using localhost:3333
0x00000000 in g_pfnVectors ()
I get a "target not yet examined" error which I don't understand. The vector table is all zeroes, so nothing has yet been placed in the RAM yet.
(gdb) load
Loading section .isr_vector, size 0x298 lma 0x0
Loading section .text, size 0x1688 lma 0x10000000
Load failed
Open On-Chip Debugger 0.10.0+dev-00546-g1afec4f-dirty (2019-02-01-13:33)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
debug_level: 1
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
3333
none separate
adapter speed: 5000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Error: Could not find MEM-AP to control the core
embedded:startup.tcl:24: Error:
in procedure 'stm32mp15x.cpu2'
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 24
undefined debug reason 7 - target needs reset
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
...
Solved! Go to Solution.
2019-07-22 12:55 AM
Thank you for your comments.
I did get there in the end. I was just lacking a little GDB knowledge (I much prefer graphical debuggers). The process is a bit laborious, but I can work out how to script it later (this is presumably what Eclipse is doing). For the benefit of others who might want to do this:
GDB halts at wherever your firmware is currently executing. To reset the firmware:
I'm sure this is not the only way to debug firmware running in production mode, and perhaps I could do it more efficiently. It's been interesting getting here: I wanted to understand what is going on with this hardware (compared to my usual domain, it's not Kansas any more). But now I wonder if I can have my cake and eat it. I don't love Eclipse for project management, and prefer text-based build systems such as CMake. On the other hand, SW4STM32 was doing a decent job of being a graphical debugger for the examples.
2019-07-20 4:39 AM
Hmm... OK. Made some progress. I can start the program via SysFS on the Linux side, and then connect to it from gdb through openocd. Still don't know how to reset the firmware. I must be missing something for it to be this much effort.
2019-07-20 4:53 AM
You can also have a look at the Bl*ckm*g*c" Debug Probe https://github.com/blacksphere/blackm*g*c/wiki , compiled for the pc-stlinkv2 Platform (make PROBE_HOST=pc-stlinkv2). For compiling, GNU tools are needed. You start the PC hosted executable and in gdb you connect to that tool wilt "target ext :2000).
Replace * by fitting vocals, as writing the names explicit gets the message rejected.
2019-07-21 11:37 PM
Hi @Community member
Copy past here interesting part of an answer you can find in following post :
You can avoid using a IDE by using directly OpenOCD and GDB provided in openSTlinux Developer Package SDK
or even using only the OpenOCD from SDK together with any GDB for ARM already available in your PC.
The wiki page below is specific for debugging the Cortex-A core, but many information on how to run OpenOCD with GDB are similar for the Cortex-M case. Please note that the OpenOCD port to connect GDB to Cortex-M is the 3333, while it is 3334 for Cortex-A.
https://wiki.st.com/stm32mpu/wiki/GDB
If you need to rebuild OpenOCD, the code is available inside the yocto recipe in
https://github.com/STMicroelectronics/meta-st-stm32mp/tree/thud/recipes-devtools/openocd
Hope it help
Olivier
2019-07-22 12:20 AM
Hi @Community member
Reading again your post, maybe also missing piece for you may be this page :
https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview
Where you can find how to load and start firmware from Linux Sysfs
Olivier
2019-07-22 12:55 AM
Thank you for your comments.
I did get there in the end. I was just lacking a little GDB knowledge (I much prefer graphical debuggers). The process is a bit laborious, but I can work out how to script it later (this is presumably what Eclipse is doing). For the benefit of others who might want to do this:
GDB halts at wherever your firmware is currently executing. To reset the firmware:
I'm sure this is not the only way to debug firmware running in production mode, and perhaps I could do it more efficiently. It's been interesting getting here: I wanted to understand what is going on with this hardware (compared to my usual domain, it's not Kansas any more). But now I wonder if I can have my cake and eat it. I don't love Eclipse for project management, and prefer text-based build systems such as CMake. On the other hand, SW4STM32 was doing a decent job of being a graphical debugger for the examples.
2019-07-31 9:17 AM
Further progress....
Using a graphical debugger is far more convenient and productive than using GDB (YMMV). After much fruitless faffing about with VSCode's launcher, I installed QtCreator and followed the instructions here: https://electronics.stackexchange.com/questions/212018/debugging-an-arm-stm32-microcontroller-using-qt-creator, with some mods for GDB startup commands. I still have to manually copy and start the firmware via Linux, and start openocd as before, but I then launch the firmware in the IDE and much is right with the world. I should have tried this sooner.
I still need to sort out the SVD or whatever to view peripheral registers, but not sure if QtCreator supports this. Maybe there's a plugin...
The IDE also understands my CMake files and executes the build exactly as Ninja does from the command line. Deep joy.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.