2019-07-01 11:48 AM
I've tried to create a bootable CD card image using both the Starter image as well as a Yocto built image. In both cases the device fails to boot.
I've gone into stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1 directory and then run:
scripts/create_sdcard_from_flashlayout.sh flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-basic.tsvThis creates a .RAW image and instruction on how to load that onto the SD card. I then run:
sudo dd if=flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/sdb bs=8M conv=fdatasync status=progressWhen this is done I insert the SD card into the stm32mp157c-dk2 board and set both boot dip switches to on. I then apply power and nothing happens. There is no output on the terminal.
Is this method supported?
2019-07-02 3:51 AM
Hi @nlbutts
Yes this is supported
Please refer to User manual to check you didn't forget any step :
https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
Hope it help
Olivier
2019-07-02 6:10 AM
Thanks for the response. I followed that page precisely and my board would not boot. I did get it to boot by using the STM32_Programmer_CLI tool. But I would like to simply image an SD card.
2019-07-03 3:02 AM
Hello, did you use a Linux PC or a VM ?
I just tried using VMware without trouble.
On VM, be sure you write to the right SD-Card and this one is visible (use cat /proc/partitions).
~/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1/scripts$ ./create_sdcard_from_flashlayout.sh
../flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-basic.tsv
Create Raw empty image: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of 1536MB
Create partition table:
[CREATED] part 1: fsbl1 [partition size 256.0 KiB]
[CREATED] part 2: fsbl2 [partition size 256.0 KiB]
[CREATED] part 3: ssbl [partition size 2.0 MiB]
[CREATED] part 4: bootfs [partition size 64.0 MiB]
[CREATED] part 5: vendorfs [partition size 16.0 MiB]
[CREATED] part 6: rootfs [partition size 750.4 MiB]
[CREATED] part 7: userfs [partition size 703.0 MiB]
Partition table from ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw
Disk ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw: 3145728 sectors, 1.5 GiB
Sector size (logical): 512 bytes
Disk identifier (GUID): 1868411E-3CF7-4736-B071-95E882E39B34
Partition table holds up to 128 entries
Main partition table begins at sector 2 and ends at sector 33
First usable sector is 34, last usable sector is 3145694
Partitions will be aligned on 2-sector boundaries
Total free space is 0 sectors (0 bytes)
Number Start (sector) End (sector) Size Code Name
1 34 545 256.0 KiB 8300 fsbl1
2 546 1057 256.0 KiB 8300 fsbl2
3 1058 5153 2.0 MiB 8300 ssbl
4 5154 136225 64.0 MiB 8300 bootfs
5 136226 168993 16.0 MiB 8300 vendorfs
6 168994 1705857 750.4 MiB 8300 rootfs
7 1705858 3145694 703.0 MiB 8300 userfs
Populate raw image with image content:
[ FILLED ] part 1: fsbl1, image: u-boot-spl.stm32-stm32mp157c-dk2-basic
[ FILLED ] part 2: fsbl2, image: u-boot-spl.stm32-stm32mp157c-dk2-basic
[ FILLED ] part 3: ssbl, image: u-boot-stm32mp157c-dk2-basic.img
[ FILLED ] part 4: bootfs, image: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 5: vendorfs, image: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 6: rootfs, image: st-image-weston-openstlinux-weston-stm32mp1.ext4
[ FILLED ] part 7: userfs, image: st-image-userfs-openstlinux-weston-stm32mp1.ext4
###########################################################################
###########################################################################
RAW IMAGE generated: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw
WARNING: before to use the command dd, please umount all the partitions
associated to SDCARD.
sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '`
To put this raw image on sdcard:
sudo dd if=../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/mmcblk0 bs=8M conv=fdatasync status=progress
(mmcblk0 can be replaced by:
sdX if it's a device dedicated to receive the raw image
(where X can be a, b, c, d, e)
###########################################################################
###########################################################################~/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1/scripts$ sudo dd if=../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/sdb bs=8M conv=fdatasync
192+0 records in
192+0 records out
1610612736 bytes (1.6 GB, 1.5 GiB) copied, 82.6478 s, 19.5 MB/sthen when you boot the DK2 platform using this SD-Card, should see on the console (ST-Link VCP)
U-Boot SPL 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.41
Trying to boot from MMC1
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in basic mode (st,stm32mp157c-dk2)
Board: MB1272 Var2 Rev.C-01
Watchdog enabled
DRAM: 512 MiB
.......
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.