2022-11-20 11:48 PM
Hi,
root@si-rd22:/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0/u-boot-stm32mp-2020.10.r1# make stm32mp15_defconfig
Makefile:40: *** missing separator. Stop.
can anyone please let me know in makefile line no. 40 I tried putting TAB but still error is not resolved.
Makefile:
else ifeq ("riscv64", $(MK_ARCH))
export HOST_ARCH=$(HOST_ARCH_RISCV64)
endif
undefine MK_ARCH // line no 40
Thankyou
Solved! Go to Solution.
2022-11-22 5:07 AM
Hello @AKuma.46 ,
You seems to be on Ecosystem v3.0. If you read the file "../README.HOW_TO.txt", you can see that the command that must be launched is:
make stm32mp15_trusted_defconfigPlease can you try again by following the readme and tell me if you still encounter errors.
For a first boot, you must not modify any Makefile or other files.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-11-22 5:07 AM
Hello @AKuma.46 ,
You seems to be on Ecosystem v3.0. If you read the file "../README.HOW_TO.txt", you can see that the command that must be launched is:
make stm32mp15_trusted_defconfigPlease can you try again by following the readme and tell me if you still encounter errors.
For a first boot, you must not modify any Makefile or other files.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-11-24 9:56 PM
Dear @Kevin HUBER
else ifeq ("riscv64", $(MK_ARCH))
export HOST_ARCH=$(HOST_ARCH_RISCV64)
endif
undefine MK_ARCH // line no 40
After Modifying line 40 to "undefine: MK_ARCH" error was resolved.
Note: We didn't modified the Makefile or other file as we were making 1st build, but still this error was encountered.
Thanks & Regards
Aniket Kumar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.